Hello. I am having issues booting from NAND on DM816x.
I believe the NAND chip should boot fine since both the ROM & NAND(i believe...) are using 8Bit ECC; 2KB page size; 128KB Block size.
That is what uboot uses according to this: http://processors.wiki.ti.com/index.php/TI81XX_PSP_UBOOT_User_Guide#U-Boot_NAND_Support
Is this true for the ROM as well?
I am using the following for MBOOT[4:0] for SD Card boot:
10110
And we are attempting to boot from NAND using:
10010
I hooked up a serial port to UART0 and can confirm it starts to print out our a character a second, which is indicative of a nand boot failure and continuing on to attempt serial boot
I have tried every combination of settings of the CSMUX to no avail
I can confirm NAND read/write operations work in Uboot with no issues (i am storing UBoot environmental variables in the nand, and they stick on reboot.)
Has anyone else had any luck getting Uboot to boot from this chip? I can dump what is stored in the NAND if need be.
Is there anyway to see why the ROM fails to boot the NAND? Some kind of log out to a console?
Currently I am flashing the NAND via Uboot. It will be difficult for me at this time to use the CCS to flash the nand since i don't have JTAG hooked up yet.
Thanks!