Hi,
can i get the details to overlock the processor and ddr with procedure, need maximum supported value, we are using EZSDK
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
can i get the details to overlock the processor and ddr with procedure, need maximum supported value, we are using EZSDK
Hello,
I would recommend you to check the TRM chapter 1.10 Device Clocking and Flying Adder PLL. Make sure that you are not exceeding the supported values fro your device.
You could look into u-boot code for better understanding of PLL configuration ( /ezsdk/board-support/u-boot-2010.06-psp04.04.00.01/board/ti/ti8168/evm.c file)
Check this wiki page :
http://processors.wiki.ti.com/index.php/TI81XX_PSP_PM_CLOCK_FRAMEWORK_User_Guide
Best Regards,
Margarita
Hi Pavel/Margarita
This is my config
TI8168-GP rev 2.1
HDVICP clk : 600MHz
L3 Fast clk : 549MHz
HDVPSS clk : 274MHz
Ducati M3 clk : 274MHz
DSP clk : 1000MHz
ARM clk : 1200MHz
DDR clk : 796MHz
i need to increase further ARM clk and DDR clk , we are using ddr3.