Dear....
I use DM8168 with 24bit RGB LCD connected in DVO2.. connected by SN75LVDS83B
I read http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/t/164800
and http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/t/360338
VOUT[0]_CLK >> CLKIN
VOUT[0]_AVID (pin=AR8) >> ENABLE
VOUT[0]_HSYNC >> HSYNC
VOUT[0]_VSYNC >> VSINC
VOUT[0] 24bitRGB >> 24bit_RGB
The pin=AR8 is muxed by
PINCTRL39 (function 1) which means "VOUT[0]_AVID (silicon revision 1.x) or DAC_HSYNC_VOUT[ 0]_AVID (silicon revision 2.x) "
Our chip revision number is "TI8168-GP rev 2.1" which is printed by u-boot
and also I read DEVICE_ID = 0x3B81E02F from DM8168, which does mean revision is "2.1"
My question is "Can I use pin AR8 as ENABLE signal for SN75LVDS83B at DM8618 revision 2.1 chip ?"
SN75LVDS83B datasheet www.ti.com/.../sn75lvds83b.pdf
Best Regards
Larry C.H Lee