Hi,
I am using the DM8168 processor with Silicon revision 2.1. The EZSDK version is 5_05_02_00 and my Linux version linux-2.6.37-psp04.04.00.01. I am using TVP5150 chip and OV7725 CMOS camera for streaming. I am using saLoopBack application to capture the same.
I have modified the application source as per my input devices. When I am trying run the application, I can able to see my streaming display in the HDMI with the resolution of 720x480 and 720x576 as well.
But I want to display my streaming in HDMI with 1080p, 720p resolution and to display the same in my LCD also (800x480).
Please let me know in which I have to change in the source code (Application / driver) to make it work for the above requirement.
Thanks in advance.
Regards,
Salih