Hi,
I am using DM8168 processor with EZSDK version of 5_05_02_00 and my Linux version is linux-2.6.37-psp04.04.00.01.
I am trying to SATA disk through PCIe. While writing some more than 100 MB, the SATA disk is resetting and I am getting below error message:
ata1.00: exception Emask 0x0 SAct 0x1 SErr 0x0 action 0x6 frozen
ata1.00: failed command: WRITE FPDMA QUEUED
ata1.00: cmd 61/08:00:00:00:00/00:00:00:00:00/40 tag 0 ncq 4096 out
res 40/00:00:00:00:00/00:00:00:00:00/00 Emask 0x4 (timeout)
ata1.00: status: { DRDY }
ata1: hard resetting link
ata1: SATA link up 6.0 Gbps (SStatus 133 SControl 300)
ata1.00: configured for UDMA/100
ata1.00: device reported invalid CHS sector 0
ata1: EH complete
Please let me know, what might be reason for this issue?
Thanks in advance.
Regards,
Salih