Hello,
I received the DM8168 Hybrid DVR from UD Works before 1 week and was following the DM8168_DVR_RDK installation guide to get the RDK demo applications running.However, during the updating Flashing U-Boot from U-Boot using Nand boot, I got interrupted, I have configured the boot mode configuration switch (SW1) for NAND boot mode with SW1[10:1] ---> 0000010010 and given TFTP Serverip as 192.168.1.100 and DVR IP Address as using DHCP command which is in a lan connection given automatically ip address as 192.168.2.23.I suspect the network domain is changed using dhcp command but my linux host machine(ubuntu 10.04) and DVR Should be in same Network domain as given in the installation guide.After that i have given "nand scrub" command because i want to program UBIFS image in further steps. Then due to some reason i have closed the U-boot prompt by closing the terminal manually.When i again setup minicom through serial port and nothing is output on the serial port when powered on.I have checked the serial port and minicom and they are working.I also checked the voltages at SW1 and they are correct. I have checked the waveform using oscilloscope at the input pin (Pin 11) of U29 (RS232 level converter) and found no waveform. So i assume there is no data coming from the Netra controller.Finally i suspect that no boot loader running/ corrupted in the DVR.
Any one please tell me correct solution to this issue as soon as possible and thanks in advance.
Thanks & Regards,
B.S.Sarath.