Hi,
While flashing UBIFS image through tftp by following DM8168_DVR_RDK Installation guide i had an error after executing "tftp 0x81000000 ubi_128_DM816X_UD_DVR.img;" as shown in the attachment. I have configured my TFTP server on Linux host machine correctly and checked to receive a file from the server it is ok. I have given TFTP Server ip as 192.168.1.100 and DVR RDK ip using static ip address as 192.168.1.180 as mentioned in the installation guide.I have connected the Ethernet cable to my Linux host PC and DVR RDK. I also done NAND scrubbing before programming ubifs image and also reprogrammed u boot and u Image before programming ubifs. I also want to know can i program the ubifs using SD card and what are necessary commands.please suggest a solution to this issue.
Thanks in Advance
Regards,