Hi friends:
I'm using "DVRRDK_04.00.00.03" to update my hardware from "DVRRDK_02.00.00.23". but the uboot-dvr-rdk can't work well.
After I write the u-boot.noxip.bin to the nand flash(K9F2G08U0C), and boot the kernel(linux-dvr-rdk in DVRRDK_04.00.00.03).
The kernel log can't print nand's info.Finally I found the kernel return with error at: nand_base.c--->nand_get_flash_type().
U-Boot 2010.06-dirty (Jul 01 2015 - 09:09:51) TI8168-GP rev 2.0 HDVICP clk : 600MHz L3 Fast clk : 549MHz HDVPSS clk : 274MHz Ducati M3 clk : 274MHz DSP clk : 1000MHz ARM clk : 987MHz DDR clk : 531MHz I2C: ready DRAM: 1 GiB NAND: HW ECC BCH8 Selected 256 MiB MMC: OMAP SD/MMC: 0 :,;;:;:;;;;;;;;r;;:,;;:;:;;;;;;;;:,;;:;:;;;;;;;;:,;;:;:;;;;;;;;:;;;;;;;;:,;;:;: ;,;:::;;;;r;;;rssiSiS552X5252525259GX2X9hX9X9XX2325S55252i5:,;;:;:;;;;;;;;:,;;: ;:;;;;;;;rrssSsS52S22h52299GGAAMHMM#BBH#B#HMM#HMBA&&XX2255S2S5Si:,;;:;:;;;;;;;; ;:;;r;;rsrrriiXS5S329&A&MH#BMB#A&9XXA252GXiSXX39AAMMMBB&G22S5i2SSiiiisi:,;;:;:; ;;;;;r;rr2iisiih393HB#B#AA99i22irrrX3X52AGsisss2Xii2299HBMA&X2S5S5iSiisSsi:,;;: r:r;rrsrsihXSi2&##MHB&Ahh3AGHGA9G9h&#H##@@@##MAMMXXX9SSS29&&HGGX2i5iisiiisisi:, ;;rrrrsSiiiA&ABH&A9GAGhAhBAMHA9HM@@@@@@@@@@@@@@@@@@@HHhAh2S2SX9&Gh22SSiisiiisii r:rrssisiS2XM##&h3AGAX&3GG3Ssr5H@M#HM2; ;2X&&&MHMB###GBB#B&XXSSs529XX55iSsisisi r;rsrisSi2XHAhX99A3XXG&&XS;:,rH#HGhAS @@@@3rs2XBM@@A552&&AHA2XiisSS252SSsisSs r;issi5S22&&3iSSX292&hXsr;;:;h@&G339&S9@@@@2@MA&9&HB##Xris29ABMAAX2ir;rsSi5iss5 rrsSi2XhG&9GXh399&X99i;;;;;;r#H&293H9X#@@@@@@@B&9GhAH@XrrsrsiXABHB&HG2rr;rrSiSi ;:rsisS599&AA9XG&3A35r;:::;,;BMh&&2iX5A@@@@@@@&392X5GB2;;;r;iSX393A##A&Xi:::rsi ;:rss552222X553&XHMhir;;::,:,h#HhGSXhG3#@@@@#AXXS2XAHA;::;;;;ss55XShBA3239r:,;; r;ii2S5SSi2i53hirsh2srr::,,,,;MMXX359&Ah3h&Si59SX99A#i:,::::;;sri2,.2r;:SGAr;,: ;:;rrrrssiriXGSi::shs;;;,,,:,,rBBA9h5s5h5iS5isi2SAHB5:,,,:::;rrs5&SrisSX5Srrr:, ;,r;;;;rsriSSrrrr;;5Xrr;;,:,,.,;9AA2SsisS5323XXXG9&i:.,,::;;r;;;srrrrrr;;:;:::: :,;r;r;rrissrrr;:;::;s;;;;,:,,..,r293h222hXXAAGGGX;:,,,:,:,::;:;::,:,,,,...,,,, ;,;;;;rrrrrrrrirr;,.,,:::::::,,,,.,;SX&ABAB2hhXir:,,.,,.,,:,,,,..,,,..,..,,,..: :.:;:;;;:;;;;r;rrs;:.. ,,:::::,:,:,,.::rrsrr;;,,.......,..,....,,,,,,,...,.,,:, :.:::,::::::;;r;rrr;:.......,.,.,,:::,,...............,,::.,,,,:,::,,:,:,,,:,;: ,.::,:,,,,,;;;;;;;;r;;::,..............................;;;:;::::,:::::::,:,:,,, : ,,:,,,,,,,,,,,,,:;rrr;;:;,,,,,,,::,.,.:.,.,;s,:;;;;:;:;;;;;::::,:::,:::,:,:,: ,.,,,,,,,...,,.,,....................................:,............:,,,:,:,,,,, Net: Detected MACID:84:7e:40:7f:d1:38 Ethernet PHY: GENERIC @ 0x01 DaVinci EMAC Hit any key to stop autoboot: 0 TI8168_EVM#print bootdelay=3 baudrate=115200 autoload=no verify=yes bootfile=uImage ramdisk_file=ramdisk.gz loadaddr=0x81000000 script_addr=0x80900000 loadbootscript=fatload mmc 0 ${script_addr} boot.scr bootscript= echo Running bootscript from MMC/SD to set the ENV...; source ${script_addr} ethaddr=84:7e:40:7f:d1:38 ethact=DaVinci EMAC bootcmd=nand read 0x81000000 0x00280000 0x296800; bootm 0x81000000 bootargs=mem=128M ddr_mem=1024M console=ttyO2,115200n8 root=/dev/mtdblock3 rw rootfstype=jffs2 ip=192.168.1.77:192.168.1.36:192.168.1.1:255.255.255.0::eth0:off vram=20M notifyk.vpssm3_sva=0xbfd00000 filesize=295F38 fileaddr=81000000 ipaddr=192.168.1.66 serverip=192.168.1.36 stdin=serial stdout=serial stderr=serial ver=U-Boot 2010.06-dirty (Jul 01 2015 - 09:09:51) Environment size: 755/131068 bytes TI8168_EVM#boot NAND read: device 0 offset 0x280000, size 0x296800 Skipping bad block 0x004c0000 2713600 bytes read: OK ## Booting kernel from Legacy Image at 81000000 ... Image Name: Linux-2.6.37+ Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 2711288 Bytes = 2.6 MiB Load Address: 80008000 Entry Point: 80008000 Verifying Checksum ... OK Loading Kernel Image ... OK OK Starting kernel ... Uncompressing Linux... done, booting the kernel. Linux version 2.6.37+ (root@ubuntu) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #48 Thu Jul 2 09:48:57 HKT 2015 CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache Machine: ti8168evm vram size = 20971520 at 0x0 ti81xx_reserve: ### Reserved DDR region @87f00000 reserved size = 20971520 at 0x0 FB: Reserving 20971520 bytes SDRAM for VRAM Memory policy: ECC disabled, Data cache writeback OMAP chip is TI8168 2.0 Built 1 zonelists in Zone order, mobility grouping on. Total pages: 27136 Kernel command line: mem=128M ddr_mem=1024M console=ttyO2,115200n8 root=/dev/mtdblock3 rw rootfstype=jffs2 ip=192.168.1.77:192.168.1.36:192.168.1.1:255.255.255.0::eth0:off vram=20M notifyk.vpssm3_sva=0xbfd00000 PID hash table entries: 512 (order: -1, 2048 bytes) Dentry cache hash table entries: 16384 (order: 4, 65536 bytes) Inode-cache hash table entries: 8192 (order: 3, 32768 bytes) Memory: 106MB 1MB = 107MB total Memory: 102188k/102188k available, 28884k reserved, 0K highmem Virtual kernel memory layout: vector : 0xffff0000 - 0xffff1000 ( 4 kB) fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) DMA : 0xffc00000 - 0xffe00000 ( 2 MB) vmalloc : 0xc8800000 - 0xf8000000 ( 760 MB) lowmem : 0xc0000000 - 0xc8000000 ( 128 MB) pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) modules : 0xbf000000 - 0xbfe00000 ( 14 MB) .init : 0xc0008000 - 0xc0042000 ( 232 kB) .text : 0xc0042000 - 0xc057e000 (5360 kB) .data : 0xc057e000 - 0xc05d7440 ( 358 kB) SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 NR_IRQS:407 IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts Total of 128 interrupts on 1 active controller GPMC revision 6.0 Trying to install interrupt handler for IRQ400 Trying to install interrupt handler for IRQ401 Trying to install interrupt handler for IRQ402 Trying to install interrupt handler for IRQ403 Trying to install interrupt handler for IRQ404 Trying to install interrupt handler for IRQ405 Trying to install interrupt handler for IRQ406 Trying to install type control for IRQ407 Trying to set irq flags for IRQ407 OMAP clockevent source: GPTIMER1 at 27000000 Hz Console: colour dummy device 80x30 Calibrating delay loop... 986.31 BogoMIPS (lpj=4931584) pid_max: default: 32768 minimum: 301 Security Framework initialized Mount-cache hash table entries: 512 CPU: Testing write buffer coherency: ok devtmpfs: initialized TI81XX: Map 0x87f00000 to 0xfe500000 for dram barrier TI81XX: Map 0x40300000 to 0xfe600000 for sram barrier omap_voltage_early_init: voltage driver support not added regulator: core version 0.5 regulator: dummy: NET: Registered protocol family 16 omap_voltage_domain_lookup: Voltage driver init not yet happened.Faulting! omap_voltage_add_dev: VDD specified does not exist! OMAP GPIO hardware version 0.1 OMAP GPIO hardware version 0.1 ti8168_evm mode HuanYi NVCT 4.2 Linux version 2.6.37+ omap_mux_init: Add partition: #1: core, flags: 0 _omap_mux_get_by_name: Could not find signal i2c2_scl.i2c2_scl _omap_mux_get_by_name: Could not find signal i2c2_sda.i2c2_sda registered ti816x_gpio_vr device ti8168_evm init ok registered ti816x_sr device Cannot clk_get ck_32 pm_dbg_init: only OMAP3 supported registered ti81xx_vpss device registered ti81xx_vidout device registered ti81xx on-chip HDMI device registered ti81xx_fb device registered ti81xx_vin device ti81xx_pcie: Invoking PCI BIOS... ti81xx_pcie: Setting up Host Controller... ti81xx_pcie: Register base mapped @0xc8820000 ti81xx_pcie: Starting PCI scan... PCI: bus0: Fast back to back transfers enabled ti81xx_pcie: PCI scan done. bio: create slab <bio-0> at 0 regulator: VFB: 800 <--> 1025 mV at 1025 mV vgaarb: loaded SCSI subsystem initialized usbcore: registered new interface driver usbfs usbcore: registered new interface driver hub usbcore: registered new device driver usb registerd cppi-dma Intr @ IRQ 17 Cppi41 Init Done omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz omap_i2c omap_i2c.2: bus 2 rev4.0 at 100 kHz Advanced Linux Sound Architecture Driver Version 1.0.23. Switching to clocksource gp timer musb-hdrc: version 6.0, host, debug=0 musb-hdrc musb-hdrc.0: dma type: dma-cppi41 musb-hdrc musb-hdrc.0: MUSB HDRC host driver musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1 usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 usb usb1: Product: MUSB HDRC host driver usb usb1: Manufacturer: Linux 2.6.37+ musb-hcd usb usb1: SerialNumber: musb-hdrc.0 hub 1-0:1.0: USB hub found hub 1-0:1.0: 1 port detected musb-hdrc musb-hdrc.0: USB Host mode controller at c881e000 using DMA, IRQ 18 musb-hdrc musb-hdrc.1: dma type: dma-cppi41 musb-hdrc musb-hdrc.1: MUSB HDRC host driver musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2 usb usb2: New USB device found, idVendor=1d6b, idProduct=0002 usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 usb usb2: Product: MUSB HDRC host driver usb usb2: Manufacturer: Linux 2.6.37+ musb-hcd usb usb2: SerialNumber: musb-hdrc.1 hub 2-0:1.0: USB hub found hub 2-0:1.0: 1 port detected musb-hdrc musb-hdrc.1: USB Host mode controller at c8826800 using DMA, IRQ 19 NET: Registered protocol family 2 IP route cache hash table entries: 1024 (order: 0, 4096 bytes) TCP established hash table entries: 4096 (order: 3, 32768 bytes) TCP bind hash table entries: 4096 (order: 2, 16384 bytes) TCP: Hash tables configured (established 4096 bind 4096) TCP reno registered UDP hash table entries: 256 (order: 0, 4096 bytes) UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) NET: Registered protocol family 1 RPC: Registered udp transport module. RPC: Registered tcp transport module. RPC: Registered tcp NFSv4.1 backchannel transport module. NetWinder Floating Point Emulator V0.97 (double precision) PMU: registered new PMU device of type 0 omap-iommu omap-iommu.0: ducati registered omap-iommu omap-iommu.1: sys registered JFFS2 version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc. msgmni has been set to 199 io scheduler noop registered io scheduler deadline registered io scheduler cfq registered (default) seed_gpio major#: 253, minor#: 0 Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0 omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1 omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2 console [ttyO2] enabled brd: module loaded loop: module loaded ahci probe: devid name is ahci ahci CAP register dump =0x6726ff81 Modified ahci CAP register dump =0x6f26ff81 ahci ahci.0: forcing PORTS_IMPL to 0x3 ahci: SSS flag set, parallel bus scan disabled ahci ahci.0: AHCI 0001.0100 32 slots 2 ports 3 Gbps 0x3 impl platform mode ahci ahci.0: flags: ncq sntf stag pm led clo only pmp pio slum part ccc scsi0 : ahci_platform scsi1 : ahci_platform ata1: SATA max UDMA/133 irq_stat 0x00000040, connection status changed irq 16 ata2: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x180 irq 16 omap2-nand driver initializing ----------omap2-nand driver initializing over-------- -------------nand_flash_dev------------ nand_get_flash_type: maf_id is ff, dev_id is ff nand_get_flash_type: second ID read is ff,ff -------------return ERR_PTR------------ davinci_mdio davinci_mdio.0: davinci mdio revision 1.6 davinci_mdio davinci_mdio.0: detected phy mask fffffffd davinci_mdio.0: probed davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown PPP generic driver version 2.4.2 PPP Deflate Compression module registered PPP BSD Compression module registered usbcore: registered new interface driver dm9601 Initializing USB Mass Storage driver... usbcore: registered new interface driver usb-storage USB Mass Storage support registered. usbcore: registered new interface driver usbserial USB Serial support registered for generic usb 1-1: new high speed USB device using musb-hdrc and address 2 usb 1-1: New USB device found, idVendor=12d1, idProduct=1573 usb 1-1: New USB device strings: Mfr=5, Product=4, SerialNumber=0 usb 1-1: Product: HUAWEI Mobile usb 1-1: Manufacturer: Huawei Technologies usbcore: registered new interface driver usbserial_generic usbserial: USB Serial Driver core USB Serial support registered for GSM modem (1-port) option 1-1:2.2: GSM modem (1-port) converter detected usb 1-1: GSM modem (1-port) converter now attached to ttyUSB0 option 1-1:2.3: GSM modem (1-port) converter detected usb 1-1: GSM modem (1-port) converter now attached to ttyUSB1 option 1-1:2.4: GSM modem (1-port) converter detected usb 1-1: GSM modem (1-port) converter now attached to ttyUSB2 option 1-1:2.5: GSM modem (1-port) converter detected usb 1-1: GSM modem (1-port) converter now attached to ttyUSB3 option 1-1:2.6: GSM modem (1-port) converter detected usb 1-1: GSM modem (1-port) converter now attached to ttyUSB4 usbcore: registered new interface driver option option: v0.7.2:USB Driver for GSM modems mice: PS/2 mouse device common for all mice rtc-ds1307 1-0068: rtc core: registered ds1337 as rtc0 omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc1 i2c /dev entries driver Linux video capture interface: v2.00 usbcore: registered new interface driver uvcvideo USB Video Class driver (v1.0.0) OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec usbcore: registered new interface driver usbhid usbhid: USB HID core driver notify_init : notify drivercreated for remote proc id 2 at physical Address 0xbfd00000 Asahi Kasei AK4104 ALSA SoC Codec Driver Cirrus Logic CS4270 ALSA SoC Codec Driver Registered tvp5158 audio codec asoc: tlv320aic3x-hifi <-> davinci-mcasp.2 mapping ok asoc: HDMI-DAI-CODEC <-> hdmi-dai mapping ok ALSA device list: #0: TI81XX SOUND0 #1: TI81XX SOUND1 TCP cubic registered NET: Registered protocol family 17 VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 omap_voltage_late_init: Voltage driver support not added Power Management for TI81XX. smartreflex smartreflex: Driver initialized rtc-ds1307 1-0068: setting system clock to 2000-04-11 05:52:38 UTC (955432358) mmc0: new high speed SDHC card at address 1234 mmcblk0: mmc0:1234 SA04G 3.63 GiB (ro) mmcblk0: p1 p2 davinci_mdio davinci_mdio.0: resetting idled controller net eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, id=282f014) IP-Config: Complete: device=eth0, addr=192.168.1.77, mask=255.255.255.0, gw=192.168.1.1, host=192.168.1.77, domain=, nis-domain=(none), bootserver=192.168.1.36, rootserver=192.168.1.36, rootpath= ata1: softreset failed (device not ready) ata1: softreset failed (device not ready) ata1: link is slow to respond, please be patient (ready=0) ata1: softreset failed (device not ready) ata1: limiting SATA link speed to 1.5 Gbps ata1: softreset failed (device not ready) ata1: reset failed, giving up ata2: SATA link down (SStatus 0 SControl 300) VFS: Unable to mount root fs via NFS, trying floppy. List of all partitions: b300 3813376 mmcblk0 driver: mmcblk b301 72261 mmcblk0p1 00000000-0000-0000-0000-000000000mmcblk0p1 b302 3735112 mmcblk0p2 00000000-0000-0000-0000-000000000mmcblk0p2 No filesystem could mount root, tried: jffs2 Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0) Backtrace: [<c0050bdc>] (dump_backtrace+0x0/0x110) from [<c03ca570>] (dump_stack+0x18/0x1c) r7:c5c00000 r6:c007a248 r5:c0030a4c r4:c05d8050 [<c03ca558>] (dump_stack+0x0/0x1c) from [<c03ca5d4>] (panic+0x60/0x17c) [<c03ca574>] (panic+0x0/0x17c) from [<c00092b4>] (mount_block_root+0x1e0/0x220) r3:00000000 r2:00000020 r1:c6429f58 r0:c04f42ec [<c00090d4>] (mount_block_root+0x0/0x220) from [<c00093a0>] (mount_root+0xac/0xcc) [<c00092f4>] (mount_root+0x0/0xcc) from [<c0009530>] (prepare_namespace+0x170/0x1d4) r4:c05d74a4 [<c00093c0>] (prepare_namespace+0x0/0x1d4) from [<c00087c4>] (kernel_init+0x114/0x154) r5:c00086b0 r4:c05d7440 [<c00086b0>] (kernel_init+0x0/0x154) from [<c007a248>] (do_exit+0x0/0x5e4) r5:c00086b0 r4:00000000
But when i use u-boot-04.04.00.01(which include in DVRRDK_02.00.00.23)boot the same kenerl
the error is gone.
ahci ahci.0: flags: ncq sntf stag pm led clo only pmp pio slum part ccc scsi0 : ahci_platform scsi1 : ahci_platform ata1: SATA max UDMA/133 irq_stat 0x00000040, connection status changed irq 16 ata2: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x180 irq 16 omap2-nand driver initializing ----------omap2-nand driver initializing over-------- -------------nand_flash_dev------------ nand_get_flash_type: maf_id is ec, dev_id is da nand_get_flash_type: second ID read is ec,da NAND device: Maf ID: 0xec, Chip ID: 0xda (Samsung, ) erasesize: 0x20000, writesize: 2048, oobsize: 64 omap2-nand: detected x8 NAND flash Creating 5 MTD partitions on "omap2-nand.0": 0x000000000000-0x000000260000 : "U-Boot" 0x000000260000-0x000000280000 : "U-Boot Env" 0x000000280000-0x0000006c0000 : "Kernel" 0x0000006c0000-0x00000cee0000 : "File System" 0x00000cee0000-0x000010000000 : "Reserved" davinci_mdio davinci_mdio.0: davinci mdio revision 1.6 davinci_mdio davinci_mdio.0: detected phy mask fffffffd davinci_mdio.0: probed davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown PPP generic driver version 2.4.2 PPP Deflate Compression module registered PPP BSD Compression module registered
I tried to modify the u-boot-dvr-rdk according u-boot-04.04.00.01, but it still had same error.
Can any one help me?