Hi All
I'm working on a custom board based on DM8168 with DVRRDK 03.50.00.05, The HDVPSS is accepting 8 bit BT656 (YUV_422) packets from the FPGA. And the audio is from AD1937 . The issue is when I start the playback of recorded video the audio and video are synchronized, here audio is leading the video. And also I noticed one more issue that audio went to off after playing the recorded video in 7 channel and 10 channel mode after few minutes ( There is no issue like this in 4 channel mode).