Hallo,
Is it possible to debug u-boot using jtag? The images I need to debug are MLO (to boot from SD) and u-boot.min.spi (to boot from SPI NOR).
Both those images are less than 128KB to be executed from internal SRAM.
which gel file do I need (if I need one)? Does the BTMODE pin have a special configuration or I can leave them untouched? Reading the u-boot elf file it seems that whole image is placed at 0x80000000 that aren't addresses in SRAM, so how can I load the elf file?
best regards
Max