Background:
Processor: AM5728
Goal: Interface to a FPGA from AM5728 via the GPMC interface.
Problem:
On boot up I see the following (dmesg | grep gpmc):
[ 0.379461] omap-gpmc 50000000.gpmc: could not find pctldev for node /ocp/l4@4a000000/scm@2000/pinmux@1400/gpmc_pins_up, deferring probe
[ 1.946078] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[ 1.951244] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 1.957527] gpiochip_add: registered GPIOs 510 to 511 on device: omap-gpmc
[ 1.957619] omap-gpmc 50000000.gpmc: cannot request GPMC CS 2
[ 1.963392] omap-gpmc 50000000.gpmc: failed to probe DT children
[ 1.969601] omap-gpmc: probe of 50000000.gpmc failed with error -16
Device Tree Configuration:
dra7.dtsi:
gpmc: gpmc@50000000 {
compatible = "ti,am3352-gpmc";
ti,hwmods = "gpmc";
reg = <0x50000000 0x37c>; /* device IO registers */
interrupts = <GIC_SPI 15 IRQ_TYPE_LEVEL_HIGH>;
dmas = <&edma_xbar 4 0>;
dma-names = "rxtx";
gpmc,num-cs = <8>;
gpmc,num-waitpins = <2>;
#address-cells = <2>;
#size-cells = <1>;
gpio-controller;
#gpio-cells = <2>;
interrupt-controller;
#interrupt-cells = <2>;
status = "disabled";
};
Our additions (in separate device tree file):
gpmc_pins_up: gpmc_pins_up {
pinctrl-single,pins = <
0x044 (PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE11) /* gpmc_a1.gpmc_a1 */
0x068 (PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE12) /* gpmc_a10.gpmc_a10 */
0x06C (PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE11) /* gpmc_a11.gpmc_a11 */
0x048 (PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE11) /* gpmc_a2.gpmc_a2 */
0x04C (PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE10) /* gpmc_a3.gpmc_a3 */
0x050 (PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE10) /* gpmc_a4.gpmc_a4 */
0x054 (PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE11) /* gpmc_a5.gpmc_a5 */
0x058 (PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE11) /* gpmc_a6.gpmc_a6 */
0x05C (PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE11) /* gpmc_a7.gpmc_a7 */
0x060 (PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE12) /* gpmc_a8.gpmc_a8 */
0x064 (PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE12) /* gpmc_a9.gpmc_a9 */
0x000 (INPUT_EN | PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE11) /* gpmc_ad0.gpmc_ad0 */
0x004 (INPUT_EN | PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE11) /* gpmc_ad1.gpmc_ad1 */
0x028 (INPUT_EN | PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE11) /* gpmc_ad10.gpmc_ad10 */
0x02C (INPUT_EN | PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE11) /* gpmc_ad11.gpmc_ad11 */
0x030 (INPUT_EN | PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE11) /* gpmc_ad12.gpmc_ad12 */
0x034 (INPUT_EN | PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE11) /* gpmc_ad13.gpmc_ad13 */
0x038 (INPUT_EN | PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE11) /* gpmc_ad14.gpmc_ad14 */
0x03C (INPUT_EN | PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE11) /* gpmc_ad15.gpmc_ad15 */
0x008 (INPUT_EN | PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE11) /* gpmc_ad2.gpmc_ad2 */
0x00C (INPUT_EN | PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE11) /* gpmc_ad3.gpmc_ad3 */
0x010 (INPUT_EN | PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE11) /* gpmc_ad4.gpmc_ad4 */
0x014 (INPUT_EN | PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE11) /* gpmc_ad5.gpmc_ad5 */
0x018 (INPUT_EN | PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE11) /* gpmc_ad6.gpmc_ad6 */
0x01C (INPUT_EN | PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE11) /* gpmc_ad7.gpmc_ad7 */
0x020 (INPUT_EN | PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE11) /* gpmc_ad8.gpmc_ad8 */
0x024 (INPUT_EN | PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE11) /* gpmc_ad9.gpmc_ad9 */
0x0C0 (INPUT_EN | PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE12) /* gpmc_clk.gpmc_clk */
0x0B8 (PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE12) /* gpmc_cs2.gpmc_cs2 */
0x0BC (PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE10) /* gpmc_cs3.gpmc_cs3 */
0x0D0 (PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE11 | MUX_MODE1) /* gpmc_ben0.gpmc_cs4 */
0x0D4 (PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE11 | MUX_MODE1) /* gpmc_ben1.gpmc_cs5 */
0x0C8 (PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE14) /* gpmc_oen_ren.gpmc_oen_ren */
0x0D8 (INPUT_EN | PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE14) /* gpmc_wait0.gpmc_wait0 */
0x0C4 (INPUT_EN | PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE13 | MUX_MODE3) /* gpmc_advn_ale.gpmc_wait1 */
0x0CC (PULL_DIS | MODE_SELECT | MUX_VIRTUAL_MODE14) /* gpmc_wen.gpmc_wen */
>;
};
&gpmc {
status = "okay";
pinctrl-names="default";
pinctrl-0 = <&gpmc_pins_up>;
ranges = <2 0 0x00000000 0x01000000>; /* fpga */
fpga {
reg = <2 0 0>;
#address-cells = <1>;
#size-cells = <0>;
gpmc,sync-clk-ps = <20000>; /* Minimum clock period for synchronous mode, in picoseconds */
gpmc,cs-on-ns = <0>; /* Assertion time */
gpmc,cs-rd-off-ns = <100> ; /* Read deassertion time */
gpmc,cs-wr-off-ns = <40>; /* Write deassertion time */
/* ADV signal timings (in nanoseconds) corresponding to GPMC_CONFIG3: */
gpmc,adv-on-ns = <0>; /* Assertion time */
gpmc,adv-rd-off-ns = <20>; /* Read deassertion time */
gpmc,adv-wr-off-ns = <20>; /* Write deassertion time */
/* WE signals timings (in nanoseconds) corresponding to GPMC_CONFIG4: */
gpmc,we-on-ns = <20>; /* Assertion time */
gpmc,we-off-ns = <20>; /* Deassertion time */
/* OE signals timings (in nanoseconds) corresponding to GPMC_CONFIG4: */
gpmc,oe-on-ns = <20>; /* Assertion time */
gpmc,oe-off-ns = <100>; /* Deassertion time */
/* Access time and cycle time timings (in nanoseconds) corresponding to GPMC_CONFIG5: */
gpmc,page-burst-access-ns = <20>; /* Multiple access word delay */
gpmc,access-ns = <80>; /* Start-cycle to first data valid delay */
gpmc,rd-cycle-ns = <120>; /* Total read cycle time */
gpmc,wr-cycle-ns = <60>; /* Total write cycle time */
gpmc,device-width = <2>; /* Total width of device(s) connected to a GPMC
chip-select in bytes. The GPMC supports 8-bit
and 16-bit devices and so this property must be
1 or 2. */
gpmc,sync-read; /* Enables synchronous read. Defaults to asynchronous is this is not set. */
gpmc,sync-write; /* Enables synchronous writes. Defaults to asynchronous is this is not set. */
};
};