Dear Team,
Currently, I'm working with linux-2.6.37-psp04.04.00.01 kernel.
Before we were using "LSI ET1011C phy" -> GMII -> 1000Mbps -> EMAC2..... It's working fine without any issue.
Now, we are changed our Ethernet phy to "Micrel ksz9031" (Just removed that PHY and connected this)
I have added ksz9031 support (ID, skew settings, pdata etc) in driver/net/phy/micrel.c and menuconfig
Now I'm able to get the PHY ID and PHY detection. While booting it's giving Link UP also but IP address is not assigned.
So, i'll try to assign the Static IP after boot. Now IP is assigned but I failed to ping.
Log file also attached.....
U-Boot 2010.06 (Nov 24 2016 - 16:33:21) TI8168-GP rev 2.1 ARM clk: 987MHz DDR clk: 796MHz I2C: ready DRAM: 1 GiB NAND: HW ECC BCH8 Selected 128 MiB MMC: OMAP SD/MMC: 0 raise: Signal # 8 caught Net: Board Info: BSP Version : iW-PRDVF-SC-01-R1.0-REL2.0-Linux2.6.37 SOM Version : iW-PRDVF-AP-01-R1.x Detected MACID:0:18:8b:b:ba:3c PHY ID = 0x221622 Ethernet PHY: KSZ9031 @ 0x03 DaVinci EMAC Hit any key to stop autoboot: 0 iW-G12M-U-Boot > iW-G12M-U-Boot > iW-G12M-U-Boot > iW-G12M-U-Boot > pri bootdelay=3 baudrate=115200 autoload=no netdev=eth0 ethprime=FEC0 loadaddr=0x81000000 kernel=uImage bootargs_base=console=ttyO2,115200n8 bootargs_nfs=setenv bootargs ${bootargs_base} root=/dev/nfs mem=364M@0x80000000 mem=320M@0x9FC00000 vmalloc=500M notifyk.vpssm3_sva=0xBF900000ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp bootcmd_net=dhcp; run bootargs_nfs;bootm bootargs_msd=setenv bootargs ${bootargs_base} root=/dev/mmcblk0p2 rootwait rw mem=364M@0x80000000 mem=320M@0x9FC00000 vmalloc=500M notifyk.vpssm3_sva=0xBF900000 ip=off noinitrd bootcmd_msd=run bootargs_msd;mmc rescan 0;fatload mmc 0 ${loadaddr} ${kernel};bootm bootcmd=run bootcmd_msd bootfile=_BOOT_FILE_PATH_IN_TFTP_ nfsroot=_ROOTFS_PATH_IN_NFS_ ethact=DaVinci EMAC ethaddr=00:18:8b:0b:ba:3c ipaddr=192.168.1.2 stdin=serial stdout=serial stderr=serial ver=U-Boot 2010.06 (Nov 24 2016 - 16:33:21) Environment size: 865/8188 bytes iW-G12M-U-Boot > ping 192.168.1.5 ### eth_halt + emac_open ## gen_auto_negotiate - emac_open Using DaVinci EMAC device ### eth_send ### eth_send ### eth_halt Abort ping failed; host 192.168.1.5 is not alive iW-G12M-U-Boot > ping 192.168.1.2 ### eth_halt + emac_open ## gen_auto_negotiate - emac_open Using DaVinci EMAC device ### eth_send ### eth_send ### eth_halt ping failed; host 192.168.1.2 is not alive iW-G12M-U-Boot > ping 192.168.1.1 ### eth_halt + emac_open ## gen_auto_negotiate - emac_open Using DaVinci EMAC device ### eth_send ### eth_send ### eth_halt ping failed; host 192.168.1.1 is not alive iW-G12M-U-Boot > boot raise: Signal # 8 caught raise: Signal # 8 caught reading uImage 2623236 bytes read ## Booting kernel from Legacy Image at 81000000 ... Image Name: Linux-2.6.37 Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 2623172 Bytes = 2.5 MiB Load Address: 80008000 Entry Point: 80008000 Verifying Checksum ... OK Loading Kernel Image ... OK OK Starting kernel ... Linux version 2.6.37 (lakshmi@lakshmi) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #3 Thu Nov 24 16:11:45 IST 2016 CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache Machine: TI-DM8168 iW-RainboW-G12M-Q7 reserved size = 52428800 at 0x0 FB: Reserving 52428800 bytes SDRAM for VRAM Memory policy: ECC disabled, Data cache writeback OMAP chip is TI8168 2.1 Built 1 zonelists in Zone order, mobility grouping on. Total pages: 160648 Kernel command line: console=ttyO2,115200n8 root=/dev/mmcblk0p2 rootwait rw mem=364M@0x80000000 mem=320M@0x9FC00000 vmalloc=500M notifyk.vpssm3_sva=0xBF900000 ip=off noinitrd PID hash table entries: 2048 (order: 1, 8192 bytes) Dentry cache hash table entries: 65536 (order: 6, 262144 bytes) Inode-cache hash table entries: 32768 (order: 5, 131072 bytes) Memory: 364MB 270MB = 634MB total Memory: 637700k/637700k available, 62716k reserved, 276480K highmem Virtual kernel memory layout: vector : 0xffff0000 - 0xffff1000 ( 4 kB) fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) DMA : 0xffc00000 - 0xffe00000 ( 2 MB) vmalloc : 0xd7000000 - 0xf8000000 ( 528 MB) lowmem : 0xc0000000 - 0xd6c00000 ( 364 MB) pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) modules : 0xbf000000 - 0xbfe00000 ( 14 MB) .init : 0xc0008000 - 0xc003c000 ( 208 kB) .text : 0xc003c000 - 0xc04f4000 (4832 kB) .data : 0xc04f4000 - 0xc053e000 ( 296 kB) SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 NR_IRQS:407 IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts Total of 128 interrupts on 1 active controller GPMC revision 6.0 Trying to install interrupt handler for IRQ400 Trying to install interrupt handler for IRQ401 Trying to install interrupt handler for IRQ402 Trying to install interrupt handler for IRQ403 Trying to install interrupt handler for IRQ404 Trying to install interrupt handler for IRQ405 Trying to install interrupt handler for IRQ406 Trying to install type control for IRQ407 Trying to set irq flags for IRQ407 OMAP clockevent source: GPTIMER1 at 27000000 Hz Console: colour dummy device 80x30 Calibrating delay loop... 986.31 BogoMIPS (lpj=4931584) pid_max: default: 32768 minimum: 301 Security Framework initialized Mount-cache hash table entries: 512 CPU: Testing write buffer coherency: ok devtmpfs: initialized regulator: core version 0.5 regulator: dummy: NET: Registered protocol family 16 OMAP GPIO hardware version 0.1 OMAP GPIO hardware version 0.1 omap_mux_init: Add partition: #1: core, flags: 0 Board Info: BSP Version : iW-PRDVF-SC-01-R1.0-REL2.0-Linux2.6.37 SOM Version : iW-PRDVF-AP-01-R1.x registered ti816x_gpio_vr device registered ti816x_lcd_pwr device registered ti816x_sr device pm_dbg_init: only OMAP3 supported registered ti81xx_vpss device registered ti81xx_vidout device registered ti81xx on-chip HDMI device registered ti81xx_fb device registered ti81xx_vin device ti81xx_pcie: Invoking PCI BIOS... ti81xx_pcie: Setting up Host Controller... ti81xx_pcie: Register base mapped @0xd7020000 ti81xx_pcie: Starting PCI scan... PCI: bus0: Fast back to back transfers enabled bio: create slab <bio-0> at 0 regulator: VFB: 800 <--> 1025 mV at 1010 mV vgaarb: loaded SCSI subsystem initialized usbcore: registered new interface driver usbfs usbcore: registered new interface driver hub usbcore: registered new device driver usb USBSS revision 4ea20809 registerd cppi-dma Intr @ IRQ 17 Cppi41 Init Done omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz Advanced Linux Sound Architecture Driver Version 1.0.23. Switching to clocksource gp timer musb-hdrc: version 6.0, otg (peripheral+host), debug=0 musb-hdrc musb-hdrc.0: dma type: dma-cppi41 MUSB controller-0 revision 4ea20800 musb-hdrc musb-hdrc.0: USB OTG mode controller at d701e000 using DMA, IRQ 18 musb-hdrc musb-hdrc.1: dma type: dma-cppi41 MUSB controller-1 revision 4ea20800 musb-hdrc musb-hdrc.1: USB OTG mode controller at d7026800 using DMA, IRQ 19 NET: Registered protocol family 2 IP route cache hash table entries: 16384 (order: 4, 65536 bytes) TCP established hash table entries: 65536 (order: 7, 524288 bytes) TCP bind hash table entries: 65536 (order: 6, 262144 bytes) TCP: Hash tables configured (established 65536 bind 65536) TCP reno registered UDP hash table entries: 256 (order: 0, 4096 bytes) UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) NET: Registered protocol family 1 RPC: Registered udp transport module. RPC: Registered tcp transport module. RPC: Registered tcp NFSv4.1 backchannel transport module. NetWinder Floating Point Emulator V0.97 (double precision) PMU: registered new PMU device of type 0 omap-iommu omap-iommu.0: ducati registered omap-iommu omap-iommu.1: sys registered highmem bounce pool size: 64 pages JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc. msgmni has been set to 705 io scheduler noop registered io scheduler deadline registered io scheduler cfq registered (default) Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0 omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1 omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2 console [ttyO2] enabled brd: module loaded loop: module loaded Uniform Multi-Platform E-IDE driver ide-gd driver 1.18 ahci ahci.0: forcing PORTS_IMPL to 0x3 ahci ahci.0: AHCI 0001.0100 32 slots 2 ports 3 Gbps 0x3 impl platform mode ahci ahci.0: flags: ncq sntf pm led clo only pmp pio slum part ccc scsi0 : ahci_platform scsi1 : ahci_platform ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x100 irq 16 ata2: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x180 irq 16 omap2-nand driver initializing NAND device: Manufacturer ID: 0xec, Chip ID: 0xf1 (Samsung ) Creating 5 MTD partitions on "omap2-nand.0": 0x000000000000-0x000000260000 : "U-Boot" 0x000000260000-0x000000280000 : "U-Boot Env" 0x000000280000-0x0000006c0000 : "Kernel" 0x0000006c0000-0x00000cee0000 : "File System" mtd: partition "File System" extends beyond the end of device "omap2-nand.0" -- size truncated to 0x7940000 0x000008000000-0x000008000000 : "Reserved" mtd: partition "Reserved" is out of reach -- disabled davinci_mdio davinci_mdio.0: davinci mdio revision 1.6 davinci_mdio davinci_mdio.0: detected phy mask fffffff7 davinci_mdio.0: probed davinci_mdio davinci_mdio.0: phy[3]: device 0:03, driver Micrel KSZ9031 Gigabit PHY usbcore: registered new interface driver cdc_ether usbcore: registered new interface driver dm9601 Initializing USB Mass Storage driver... usbcore: registered new interface driver usb-storage USB Mass Storage support registered. mice: PS/2 mouse device common for all mice input: max11801_ts as /devices/platform/omap/omap_i2c.1/i2c-1/1-0049/input/input0 omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0 i2c /dev entries driver Linux video capture interface: v2.00 usbcore: registered new interface driver uvcvideo USB Video Class driver (v1.0.0) OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec usbcore: registered new interface driver usbhid usbhid: USB HID core driver notify_init : notify drivercreated for remote proc id 2 at physical Address 0xbf900000 usbcore: registered new interface driver snd-usb-audio asoc: tlv320aic3x-hifi <-> davinci-mcasp.2 mapping ok asoc: HDMI-DAI-CODEC <-> hdmi-dai mapping ok ALSA device list: #0: Dummy 1 #1: TI81XX EVM TCP cubic registered NET: Registered protocol family 17 VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 omap_voltage_late_init: Voltage driver support not added Power Management for TI81XX. smartreflex smartreflex: Driver initialized omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800) ata1: SATA link down (SStatus 0 SControl 300) ata2: SATA link down (SStatus 0 SControl 300) Waiting for root device /dev/mmcblk0p2... mmc0: new high speed SDHC card at address 0007 mmcblk0: mmc0:0007 SS08G 7.21 GiB mmcblk0: p1 p2 EXT3-fs: barriers not enabled kjournald starting. Commit interval 5 seconds EXT3-fs (mmcblk0p2): using internal journal EXT3-fs (mmcblk0p2): mounted filesystem with writeback data mode VFS: Mounted root (ext3 filesystem) on device 179:2. devtmpfs: mounted Freeing init memory: 208K INIT: version 2.86 booting Please wait: booting... Starting udev udevd (64): /proc/64/oom_adj is deprecated, please use /proc/64/oom_score_adj instead. Remounting root file system... Caching udev devnodes NET: Registered protocol family 10 ALSA: Restoring mixer settings... Configuring network interfaces... net eth0: attached PHY driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=0:03, id=221622) PHY READY STATE ADDRCONF(NETDEV_UP): eth0: link is not ready udhcpc (v1.13.2) started Sending discover... emac_update_phystatus - PHY Link ON PHY: 0:03 - Link is Up - 10/Half ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready Sending discover... Sending discover... No lease, forking to background done. Setting up IP spoofing protection: rp_filter. Tue Apr 14 11:57:00 UTC 2015 INIT: Entering runlevel: 5 Loading HDVICP2 Firmware DM816X prcm_config_app version: 2.0.0.1 Doing PRCM settings... PRCM for IVHD0 is in Progress, Please wait..... BW Phy Addr : 0x48180600 Data : 0x00000002 AW Phy Addr : 0x48180600 Data : 0x00000002 Phy Addr : 0x48180c04 Data : 0x00000037 BW Phy Addr : 0x48180620 Data : 0x00070000 AW Phy Addr : 0x48180620 Data : 0x00070002 BW Phy Addr : 0x48180624 Data : 0x00030000 AW Phy Addr : 0x48180624 Data : 0x00010002 Phy Addr : 0x48180600 Data : 0x00000102 BW Phy Addr : 0x48180c10 Data : 0x00000007 AW Phy Addr : 0x48180c10 Data : 0x00000003 Phy Addr : 0x48180c14 Data : 0x00000004 BW Phy Addr : 0x58088000 Data : 0x5d93076a AW Phy Addr : 0x58088000 Data : 0xeafffffe BW Phy Addr : 0x58098000 Data : 0x85175ec4 AW Phy Addr : 0x58098000 Data : 0xeafffffe BW Phy Addr : 0x48180c10 Data : 0x00000003 AW Phy Addr : 0x48180c10 Data : 0x00000000 Phy Addr : 0x48180c14 Data : 0x00000007 PRCM for IVHD0 is Done Successfully PRCM for IVHD1 is in Progress, Please wait..... BW Phy Addr : 0x48180700 Data : 0x00000002 AW Phy Addr : 0x48180700 Data : 0x00000002 Phy Addr : 0x48180d04 Data : 0x00000037 BW Phy Addr : 0x48180720 Data : 0x00070000 AW Phy Addr : 0x48180720 Data : 0x00050002 BW Phy Addr : 0x48180724 Data : 0x00030000 AW Phy Addr : 0x48180724 Data : 0x00010002 Phy Addr : 0x48180700 Data : 0x00000102 BW Phy Addr : 0x48180d10 Data : 0x00000007 AW Phy Addr : 0x48180d10 Data : 0x00000003 Phy Addr : 0x48180d14 Data : 0x00000004 BW Phy Addr : 0x5a088000 Data : 0xb8df3c75 AW Phy Addr : 0x5a088000 Data : 0xeafffffe BW Phy Addr : 0x5a098000 Data : 0x32891690 AW Phy Addr : 0x5a098000 Data : 0xeafffffe BW Phy Addr : 0x48180d10 Data : 0x00000003 AW Phy Addr : 0x48180d10 Data : 0x00000000 Phy Addr : 0x48180d14 Data : 0x00000007 PRCM for IVHD1 is Done Successfully PRCM for IVHD2 is in Progress, Please wait..... BW Phy Addr : 0x48180800 Data : 0x00000002 AW Phy Addr : 0x48180800 Data : 0x00000002 Phy Addr : 0x48180e04 Data : 0x00000037 BW Phy Addr : 0x48180820 Data : 0x00070000 AW Phy Addr : 0x48180820 Data : 0x00050002 BW Phy Addr : 0x48180824 Data : 0x00030000 AW Phy Addr : 0x48180824 Data : 0x00010002 Phy Addr : 0x48180800 Data : 0x00000102 BW Phy Addr : 0x48180e10 Data : 0x00000007 AW Phy Addr : 0x48180e10 Data : 0x00000003 Phy Addr : 0x48180e14 Data : 0x00000004 BW Phy Addr : 0x53088000 Data : 0xe8684fe2 AW Phy Addr : 0x53088000 Data : 0xeafffffe BW Phy Addr : 0x53098000 Data : 0xbb94c9c4 AW Phy Addr : 0x53098000 Data : 0xeafffffe BW Phy Addr : 0x48180e10 Data : 0x00000003 AW Phy Addr : 0x48180e10 Data : 0x00000000 Phy Addr : 0x48180e14 Data : 0x00000007 PRCM for IVHD2 is Done Successfully PRCM Initialization completed SysLink version : 2.20.02.20 SysLink module created on Date:Dec 26 2012 Time:11:03:34 FIRMWARE: I2cInit will be done by M3 FIRMWARE: Memory map bin file not passed Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [-mmap <memory_map_file>] [-i2c <0|1>] ===Mandatory arguments=== <Processor Id> 0: DSP, 1: Video-M3, 2: Vpss-M3 <Location of Firmware> firmware binary file <start|stop> to start/stop the firmware ===Optional arguments=== -mmap input memory map bin file name -i2c 0: i2c init not done by M3, 1(default): i2c init done by M3 FIRMWARE: isI2cInitRequiredOnM3: 1 FIRMWARE: Default memory configuration is used Firmware Loader debugging not configured Default FL_DEBUG: warning Allowed FL_DEBUG levels: error, warning, info, debug, log MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.2.1 FIRMWARE: 1 start Successful Loading HDVPSS (V4L2) Firmware FIRMWARE: Memory map bin file not passed Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [-mmap <memory_map_file>] [-i2c <0|1>] ===Mandatory arguments=== <Processor Id> 0: DSP, 1: Video-M3, 2: Vpss-M3 <Location of Firmware> firmware binary file <start|stop> to start/stop the firmware ===Optional arguments=== -mmap input memory map bin file name -i2c 0: i2c init not done by M3, 1(default): i2c init done by M3 FIRMWARE: isI2cInitRequiredOnM3: 0 FIRMWARE: Default memory configuration is used Firmware Loader debugging not configured Default FL_DEBUG: warning Allowed FL_DEBUG levels: error, warning, info, debug, log MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.2.1 FIRMWARE: 2 start Successful VPSS_FVID2: M3 firmware version 0x1000145 is newer,driver may not work properly. HDMI W1 rev 2.0 HDMI CEC Spec version 1.2 I2C No Ack Starting system message bus: dbus. Starting telnet daemon. Starting syslogd/klogd: done Starting thttpd. Starting PVR Starting Matrix GUI application. zero gadget: Gadget Zero, version: Cinco de Mayo 2008 zero gadget: zero ready musb-hdrc musb-hdrc.0: MUSB HDRC host driver musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1 usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 usb usb1: Product: MUSB HDRC host driver usb usb1: Manufacturer: Linux 2.6.37 musb-hcd usb usb1: SerialNumber: musb-hdrc.0 hub 1-0:1.0: USB hub found hub 1-0:1.0: 1 port detected usb 1-1: new high speed USB device using musb-hdrc and address 2 usb 1-1: device v0424 p2514 is not supported usb 1-1: New USB device found, idVendor=0424, idProduct=2514 usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0 hub 1-1:1.0: USB hub found hub 1-1:1.0: 4 ports detected tvp5150 1-005d: chip found @ 0xba (OMAP I2C adapter) tvp5150 1-005d: *** unknown tvp8081 chip detected. tvp5150 1-005d: *** Rom ver is 130.131 ti81xxvin ti81xxvin: registered sub device tvp5150 ov7725 1-0021: chip found @ 0x42 (OMAP I2C adapter) ov7725 1-0021: Product ID error a:b ov7725 1-0021: *** unknown OV7725 chip detected. ov7725: probe of 1-0021 failed with error -22 ti81xxvin ti81xxvin: Error registering v4l2 subdevice insmod: error inserting 'ti81xxvin.ko': -1 No such device Selected Device is LCD Changing Resolution to 800x480 Stopping Matrix GUI application. Stopping PVR Starting PVR Removing stale PID file /var/run/matrix-gui-e.pid. Starting Matrix GUI application. Rootfs Version : iW-PRDVF-SC-01-R1.0-REL2.0-Rootfs iWave-G12M login: root root@iWave-G12M:~# root@iWave-G12M:~# root@iWave-G12M:~# ifconfig eth0 down root@iWave-G12M:~# root@iWave-G12M:~# root@iWave-G12M:~# ifconfig eth0 192.168.1.2 up net eth0: attached PHY driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=0:03, id=221622) PHY READY STATE ADDRCONF(NETDEV_UP): eth0: link is not ready root@iWave-G12M:~# emac_update_phystatus - PHY Link ON PHY: 0:03 - Link is Up - 10/Half ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready root@iWave-G12M:~# root@iWave-G12M:~# root@iWave-G12M:~# ifconfig eth0 Link encap:Ethernet HWaddr D0:FF:50:91:C1:28 inet addr:192.168.1.2 Bcast:192.168.1.255 Mask:255.255.255.0 inet6 addr: fe80::d2ff:50ff:fe91:c128/64 Scope:Link UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:20 errors:0 dropped:0 overruns:0 carrier:9 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:5656 (5.5 KiB) Interrupt:44 Base address:0x8000 lo Link encap:Local Loopback inet addr:127.0.0.1 Mask:255.0.0.0 inet6 addr: ::1/128 Scope:Host UP LOOPBACK RUNNING MTU:16436 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:0 RX bytes:0 (0.0 B) TX bytes:0 (0.0 B) root@iWave-G12M:~# root@iWave-G12M:~# ping 192.168.1.1 PING 192.168.1.1 (192.168.1.1): 56 data bytes --- 192.168.1.1 ping statistics --- 7 packets transmitted, 0 packets received, 100% packet loss root@iWave-G12M:~# ifc -sh: ifc: not found root@iWave-G12M:~# ifconfig eth0 Link encap:Ethernet HWaddr D0:FF:50:91:C1:28 inet addr:192.168.1.2 Bcast:192.168.1.255 Mask:255.255.255.0 inet6 addr: fe80::d2ff:50ff:fe91:c128/64 Scope:Link UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:26 errors:0 dropped:0 overruns:0 carrier:15 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:6016 (5.8 KiB) Interrupt:44 Base address:0x8000 lo Link encap:Local Loopback inet addr:127.0.0.1 Mask:255.0.0.0 inet6 addr: ::1/128 Scope:Host UP LOOPBACK RUNNING MTU:16436 Metric:1 RX packets:6 errors:0 dropped:0 overruns:0 frame:0 TX packets:6 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:0 RX bytes:672 (672.0 B) TX bytes:672 (672.0 B) root@iWave-G12M:~# root@iWave-G12M:~# root@iWave-G12M:~# ping 192.168.1.1 PING 192.168.1.1 (192.168.1.1): 56 data bytes
What may be the issue ? Is anything required to do in EMAC side ? What I missed ?
Please help me.
Thanks in Advance.
Regards,
J.P.Raja