Using DM8168 at 1080p resolution is there a way to output all 30/32 bit color without the Alpha channel being stripped? Looking for suggestion on what is possible and having Alpha information at a pixel level. Some idea that I thought of but still need confirmation if possible or other suggestion:
1. Output in a 16bit packet mode but would that result in resolution dimension exceeding the HW and/or pixel clock speed?
2. Synchronize DVO1 and DVO2 output? Is that possible?
The Compositor is not used, the HDVPSS is just a pass through interface, no features utilized.
Thanks.