Other Parts Discussed in Thread: PCA9518
Hi
my company use one TMS320DM8168 processor with NAND flash MT29F8G08ABABAWP-IT B.
the processor must start from NAND flash but often it's doesn't work.
often we see at power up, some signal on the !CE of flash but the system don't start (we don't see with minicom the Uboot start print).
after 30/40 seconds, DaVinci retry to read on NAND Flash and often the boot start (we see the UBoot start print).
sometime, the system doesn't work and it retry afer 30/40 seconds.
we use boot configuration like 10011 (NAND, NANDI2C, SD, UART) but we don't have any other memory for boot
if we insert one bootable SD, sometime start from NAND, sometime start from SD (because dont find valid image on NAND flash)
how many time DaVinci wait to retry NAND flash ?
why the DaVinci don't read valid image from NAND flash often (and when retry this image is valid) ?
I see the
thanks
gianfranco