• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » DaVinci™ Video Processors » DM816x, C6A816x and AM389x Processors Forum » All Tags » 1080p
Share
DaVinci™ Video Processors
  • Forums
  • Announcements

Browse by Tags

DaVinci™ Video Processors

Welcome to the DaVinci™ Video Processors Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
1080p
  • 'DM8168
  • 1080i
  • 1080p h264
  • 1080p/30 encode
  • 8168
  • 8168 1080p capture
  • 8168 c6accel code engine
  • 8168 codec h263
  • 8168 codec h264
  • 8168 codec h264 runtime
  • 8168 codecs
  • 8168 debug
  • 8168 dvr rdk
  • 8168 DVR_RDK
  • 8168 evm
  • 8168 EZSDK
  • 8168 ezsdk omx
  • 8168EVM RDK
  • 816x
  • 816X example
  • 816x vpss
  • 81xx
  • dm8168
  • dm81xx
  • V4L2
Related Posts
  • Forum Post: gstreamer could not negotiate format for 1080p25 & 720p50

    sadasivappa s sadasivappa s
    Hello, I am working on DM816x-EVM(Netra) based custom board. Custom board setup is as following: We have DM816x Video ports connected to FPGA logic. At video RX side FPGA will recieve video from HD-SDI and converts it to 1080p30/1080p25/720p50 format and feed to VIN0 (x16) of DM816x. At video...
    on Sep 12, 2012
  • Forum Post: How to redirect video feed from HDMI RX to HDMI TX

    shakthi pradeep shakthi pradeep
    Hi, We are planning to use DM8168 in our design which would be used to perform the following. 1) Our design with have one HMDI RX port and Two HDMI TX ports. Stream from HDMI RX has to be split into two halves and each half has to be sent over the two HDMI TX ports 2) Video from the HDMI RX port...
    on Jul 18, 2012
  • Forum Post: Three video streams at 1080p60?

    MRI MRI
    How can you do three 1080p60 streams with two video input ports? If you split the ports to 8 bits, you can't do 1080p60 with an 8 bit bus at 165 MHz. Please explain?
    on Aug 31, 2012
  • Forum Post: RE: 816x Expansion I/O daughtercard: Which Inputs are supported by SDK?

    sadasivappa s sadasivappa s
    Hello HardikShah, I am working on DM816x-EVM(Netra) based custom board. Custom board setup is as following: We have DM816x Video ports connected to FPGA logic. At video RX side FPGA will recieve video from HD-SDI and converts it to 1080p30/1080p25/720p50 format and feed to VIN0 (x16) of DM816x...
    on Sep 12, 2012
  • Forum Post: DM816x: H.264 decoder bit rate

    sweta bhatt sweta bhatt
    Hi, I wanted to know whether DM816x H.264 decoder is dependent of video bit rate parameter or not. I have a requirement as below 1) to decode 4 1080p/ 4 1080i encoded streams at 15 Mbps. Is there any constraint/limitation to support maximum bit rate for each HD channel? 2) to decode 16 SD resolutions...
    on Sep 28, 2012
  • Forum Post: RE: Capture video when incoming video resolution changes on the fly

    Michael Erdahl Michael Erdahl
    Tiebing, Please have a look at this: http://processors.wiki.ti.com/index.php/TI81XX_PSP_VIDEO_CAPTURE_Driver_User_Guide#Querying_DV_preset There is code there to query current input resolution detected by the decoder. You'll need to get the file descriptor of the input stream, /dev/video0...
    on Oct 1, 2012
  • Forum Post: How to Exit gracefully while omx didnot work normally?

    feng xiao ming feng xiao ming
    Plateform:DM8168+EZSDK5.05 I run the decode_display_a8host_debug.xv5T example,but it blocked,and cannot be killed by CTRL+C. How to solve this problem, let the omx examples Exit gracefully? root@dm816x-evm:/home# ./decode_display_a8host_debug.xv5T -i 1080P_HP.h264 -w 19 20 -h 1080 -f 60 -g 0 -d...
    on Nov 2, 2012
  • Forum Post: RE: Is there an ERROR on evm816xiodc_Schematics_RevC pin connections?

    David Soto David Soto
    Hi Hardik, After get the dual capture working and test it with the saLoopBack application I started with gstreamer, mainly I wanted to run two different pipelines, each pipeline capturing from a different port. However, I found that gstreamer is having problems to work properly in this case, basically...
    on Feb 19, 2013
  • Forum Post: RE: Video Capture DM816x VIN1 BT656

    David Soto David Soto
    Hi Brijesh, Yes, I would suppose that that value 0x00000414 means an overflow on the port (not sure what means each bit on this register), however, this overflow is being caused by the absence of the SoG signal, because using gstreamer with the SoG enabled I can use the pipeline without problems and...
    on Mar 4, 2013
  • Forum Post: RE: Video Capture DM816x VIN1 BT656

    David Soto David Soto
    Hi Brijesh, Thanks for your comments. For the time being I am using a very simple pipeline which works when the SoG signal is enabled, also I am not using OMX to capture since I am using the V4L2 capture driver: gst-launch v4l2src device=/dev/video0 always-copy=false queue-size=8 ! 'video/x-raw...
    on Mar 8, 2013
  • Forum Post: How can I do video overlay after encode from HD camera and then stream out to network using rtp

    baochang wang baochang wang
    Hi, I'm using the Z3-DM8168-RPS system, it can stream in from HD camera, and stream out by network using rtp, Is someboay can tell me how can I draw some graphics on the video before stream out? I tried many ways based on TI EZSDK. but i'm not sucess. please help. thanks
    on May 2, 2013
  • Forum Post: Extending DM8168 1920x1080 (8bit) capabilities

    David Aviv David Aviv
    Hello, Following a previous conversation on this matter, I have understood that the DM8168 has an hardware limitation for video in (line length of 1920 bytes). Since I'm using an imaging sensor of 10 bits, which is extremely important for DSP purposes, I need to transfer line of 1920 of 10 bits...
    on May 20, 2013
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use