• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » DaVinci™ Video Processors » DM816x, C6A816x and AM389x Processors Forum » All Tags » 8168 DVR_RDK
Share
DaVinci™ Video Processors
  • Forums
  • Announcements

Browse by Tags

DaVinci™ Video Processors

Welcome to the DaVinci™ Video Processors Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
8168 DVR_RDK
  • 'DM8168
  • 8148
  • 814x
  • 814x EZSDK
  • 814x ezsdk omx
  • 8168
  • 8168 codecs
  • 8168 debug
  • 8168 dvr rdk
  • 8168 DVR_RDK demo
  • 8168 evm
  • 8168 EZSDK
  • 8168 ezsdk omx
  • 8168 RDK
  • 8168 RDK mcfw DSP
  • 8168EVM RDK
  • 816x
  • 816x decode
  • 816X example
  • 816x hdvpss
  • 816x rdk
  • 816x vpss
  • AM3894
  • DSP
  • Encoder
Related Posts
  • Forum Post: RE: McFW demo

    Holger Eberhard102906 Holger Eberhard102906
    Hi Brett, thanks for the information. I will get it from our FAE. Best regards Holger
    on Jun 19, 2012
  • Forum Post: h263 encoder setting

    eager hsu eager hsu
    hi,I meet a problem. have someone to help me? I use DVRRDK version 02.00.00.23 to test codec. because DVRRDK do not support mpeg4 encoding and h263 encoding,I add some code and integrate REL.500.V.MPEG4.E.SP.IVAHD.01.00.00.05 to enc link to let DVRRDK encoding mpeg4 and h.263. the application can...
    on Jun 21, 2012
  • Forum Post: 720p capture_dei_encode OMTB Script

    Michael Ortiz Michael Ortiz
    Hello, So I am trying to convert /usr/share/ti/ti-omtb/capture_dei_encode.oms to work with a 720p component source. I have made all the obvious changes such as changing the resolution values from 1920 --> 1280 and 1080 --> 720 and changing the buffer sizes proportionately. I have also changed...
    on Jun 20, 2012
  • Forum Post: RE: DVR_RDK / McFW / Vdis_switchActiveQueue()

    Holger Eberhard102906 Holger Eberhard102906
    Thank You Yogesh for this information Regards Holger
    on Jun 27, 2012
  • Forum Post: RE: kernel halt when rebooting over 1000 times on DM1816x

    Jason9296 Jason9296
    Thanks Emil. Sorry for late reply, because I had doing some experiments in these days. I had done two experiments : One is to use software watchdog timeout instead of reset system call. And use a script to run init.sh and load.sh to load firmware but do not involve any other applications. ...
    on Jun 29, 2012
  • Forum Post: DVRRDK AVSYNC ERROR on MCFW DEMO

    Liddell Chen Liddell Chen
    I'm using dvrrdk 2.80.00.10 on my board. It use a TVP5158 to capture 4 D1 CVBS input. When I choose "6: VCAP + VDIS - NO Encode or Decode",the HDMI display began to flash and get the err message: [m3vpss ] AVSYNC:WallTime IGNORE Unexpected Discontinuity.PrevTs[244901]/CurTs[245078]...
    on Jul 2, 2012
  • Forum Post: kernel halt when rebooting over 1000 times on DM1816x

    Jason9296 Jason9296
    Hi, all I am developing projects in DM8168 with slicion revision 2.0 on our customer boards. During developing, i face one strange issue that system halted randomly after rebooting. So i start to do a simple test, using a script to run init.sh and load.sh to load firmware but do not involve any...
    on Jun 19, 2012
  • Forum Post: RE: Failure on rotation/mirroring the video by use the TILER on DM8168

    Holger Eberhard102906 Holger Eberhard102906
    Hi, we have the same issue. Has anybody found a solution for mirroring video with DM8168 ? Best regards
    on Jul 9, 2012
  • Forum Post: Syslink porting guide

    Shahzad Muzaffar Shahzad Muzaffar
    Hi, We are porting Mentor Nucleus RTOS over arm. But we are facing much problems related to syslink porting and integration. Is there any Syslink porting guide? DSP link was some straight forward structure but syslink is much different in different ways and we are getting much problem in porting...
    on Jul 12, 2012
  • Forum Post: Kernel Panic while running program using mcfw of DVRRDK-02.80.00.10

    ChengYeh Yu ChengYeh Yu
    Hi: When running a program using mcfw of DVRRDK-02.80.00.10 to show the live view of a IP-Cam, this message shows up: BUG: Bad page map in process vsc_dm8168 pte:fb00a14d pmd:86e40031 and followed by the following kernel Oops Do anyone know what may be wrong? [ 2409.270000] BUG: Bad page map...
    on Jul 18, 2012
  • Forum Post: RE: Kernel Panic while running program using mcfw of DVRRDK-02.80.00.10

    ChengYeh Yu ChengYeh Yu
    Thanks for replaying. I sorry, It is "vram=20M notifyk.vpssm3_sva=0xBFD00000" I copied and pasted this bootarg from the putty (a terminal program I am using) without check it again. Here is the result of cat /proc/cmdline mem=128M mem=1020M@0xC0000000 vmalloc=1128M root=/dev/mtdblock5...
    on Jul 19, 2012
  • Forum Post: About the EMAC of DM8167

    Felix76837 Felix76837
    There are two EMACs in chip of DM8167,but i only need one of them.I look through the datasheet but i can't find out if i don't use EMAC1,what should i do with the pins of EMAC1.Can i leave these pins float?
    on Jul 20, 2012
  • Forum Post: RE: dsp develop on dm8168 using dvrrdk kit

    Xavier15128 Xavier15128
    hi, i see the "Software On-Screen Display on C674x Application Programming Interface and User’s Guide ", it shows that Application can change this value but need to make sure to rebuild the DSP firmware dvr_rdk_fw_c6xdsp.xe674. Then how to build DSP firmware dvr_rdk_fw_c6xdsp.xe674...
    on Jul 23, 2012
  • Forum Post: mcfw example

    liu jiang liu jiang
    Hi; env: DVRRDK_01_09_00_19 dm8168 when I use the dec_dis demo, it only work a few seconds. The api "Int32 Vdec_requestBitstreamBuffer(VDEC_BUF_REQUEST_S * bufReq, VCODEC_BITSBUF_LIST_S *pBitsBufList, UInt32 timeout)",couldn't get any bufs a few seconds later. Is the dec not...
    on Jul 24, 2012
  • Forum Post: DM816x EVM & McFWMcF

    y amiram y amiram
    Hello, I use the “DM816x Evaluation Module”, and run an OMX application over it. I need to switch to McFW, or direct Link component. From which version McFW support DM816x EVM? Are there sum instructions to program, build and load image built using McFW to DM816x EVM? Thanks...
    on Jul 30, 2012
  • Forum Post: Hi, I want to download C6A8168 kernel image.

    Sangyun Yun Sangyun Yun
    Hi. I have a question. I got EZSDK for DM816x. So I have DM816x kernel image. But it don't exist C6A816x kernel image. Where can I download C6A816x kernel image?
    on Jul 31, 2012
  • Forum Post: RE: Kernel crash when dm8168 connect to ipcam with special phy.

    Jason9296 Jason9296
    Hi, all, Sorry for don't clearly describe the second test. In that test, DM8168 didn't connected to any IPNC, and connected to network directly. The method I used was to reboot DM8168 repetitively by using software watchdog (force to timeout). And crash was happening frequently as previous...
    on Jul 31, 2012
  • Forum Post: SCD/Tamper Detection

    Ivan Nardi Ivan Nardi
    Hi guys, I have some troubles with SCD/tamper Detection in the latest RDK If I use RDK 02.00.00.24 , it seems to work (I see line [TAMPER DETECTED]... in the console), while if I use RDK 02.80.00.10 , it seems not. Motion Detection works with both RDKs The setup is the same in both cases: demo 1, used...
    on Jul 13, 2012
  • Forum Post: Kernel crash when dm8168 connect to ipcam with special phy.

    Jason9296 Jason9296
    Hi, all: I am developing projects in DM8168 with silicon revision 2.0 on our customer boards. And the firmware work version that I used is DVRRDK-02.00.00.23. The problem is DM8168 will crash in kernel when directly connect to our IP-Camera with special phy which part number is “ Micrel...
    on Jun 29, 2012
  • Forum Post: RE: Kernel crash when dm8168 connect to ipcam with special phy.

    Jason9296 Jason9296
    Hi, ChengYeh, Thank you for quickly reply. Our system has 1G physical memory and use config_1G_256MLinux.bld file, but because of dsp requirement we have modify this file a little bit. Please refer to the attached file. And we have try other config "CONFIG_VMSPLIT_2G=y", and use the...
    on Aug 3, 2012
  • Forum Post: AM389x LPDDR and JTAG

    Kshitij Kumar Kshitij Kumar
    Hi All I am planning a new design using AM3894 processor. I have couple of questions. 1. Is LPDDR interface possible with AM3894? I went through the datasheet and TRM, there all the references are with respect to DDR2 or DDR3. I actually wanted to use a MCP in my design, with NAND flash and...
    on Aug 13, 2012
  • Forum Post: dsp develop on dm8168 using dvrrdk kit

    Xavier15128 Xavier15128
    Hi, we do our development on dm8168 evm board, and dvrrdk_02_08_ develop kit is used, the question is that i can not find any useful information about how to do dsp development on dm8168 evm board. Though the osd link and scd link demo is supplied. Should the osd and scd algorithm developped using...
    on Jun 20, 2012
  • Forum Post: Building Syslink DSP(slave) side sample binaries

    Shahzad Muzaffar Shahzad Muzaffar
    hi, I am trying to build Syslink DSP side application binaries to test my Syslink integration with HLOS based RTOS. I have the following confusions that are not clear from documentation: 1- "CGT_C674_ELF_INSTALL_DIR" where to find these and i want to build it witout EZSDK using other tool...
    on Aug 13, 2012
  • Forum Post: Remove HDVICP2 in kernel

    Sangyun Yun Sangyun Yun
    Hi, We use C6A8168 CPU now. We make boards with C6A8168. Not DM8168. I know that DM816x is pin compatible with C6A816x. But I have a problem. HDVICP2 is loading when U-boot file call kernel image. DM816x hasn't errors because it has HDVICP2. But C6A816x hasn't HDVICP2, so it has...
    on Aug 4, 2012
  • Forum Post: rdk mcfw

    liu jiang liu jiang
    root@dvr :~# ./gui.sh *** Bootargs Validated for mem param *** *** Bootargs Validated for notifyk.vpssm3 params *** Kernel bootargs validated numid=1,iface=MIXER,name='PCM Playback Volume' ; type=INTEGER,access=rw---R--,values=2,min=0,max=127,step=0 : values=127,127 | dBscale-min=-63.50dB,step...
    on Jul 26, 2012
12345»
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use