• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » DaVinci™ Video Processors » DM816x, C6A816x and AM389x Processors Forum » All Tags » HDVPSS DM8168
Share
DaVinci™ Video Processors
  • Forums
  • Announcements

Browse by Tags

DaVinci™ Video Processors

Welcome to the DaVinci™ Video Processors Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
HDVPSS DM8168
  • 8168
  • 816x
  • AM389x
  • C6A8168
  • C6A816X
  • DaVinci
  • dm8148
  • dm8168
  • DM816x
  • DM816x C6A816x AM389x
  • dm8186
  • EzSDK
  • EZSDK 5.02
  • EzSDK 5.03
  • HDVPSS
  • Linux
  • Netra
  • omx
  • openmax
  • PSP
  • syslink
  • TI816X
  • TI81XX
  • video capture
  • VPSS
Related Posts
  • Forum Post: Re: Where can i get the hdvpss?

    Eric Mao Eric Mao
    Hi where and how can i get the HDVPSS source package. I've bought a DM8168 DVR, but the HDVPSS under the SW SDK is just part of the whole HDVPSS, some files introduce in the pdf documents is not exist, so i want to get a hdvpss install file. Can you tell me how can i get it.
    on Aug 4, 2011
  • Forum Post: Re: OMX/OMTB/VFCC: Is a plain vanilla video capture and display possible without using the TVP component?

    Juan Solis Juan Solis
    Marcus Cooksey Assuming you configure the video decoder outside the scope of OMX/OMTB then it should be possible to perform capture without the tvp and thus you can remove the tvp comment from the script. Thanks for the reply Marcus. I went ahead and tried it and the script runs without errors...
    on Aug 4, 2011
  • Forum Post: Re: Where can i get the hdvpss?

    Eric Mao Eric Mao
    Thanks for reply, I'll contact with the local FAE.
    on Aug 8, 2011
  • Forum Post: Where can i get the hdvpss?

    Eric Mao Eric Mao
    I install a ezsdk, and there is no hdvpss folder under the ezsdk, where can i get the hdvpss install file?
    on Aug 4, 2011
  • Forum Post: DM8168 custom video decoder

    Ben Tucker Ben Tucker
    Hi All, I'm working with the following hw and sw components: Hardware: Z3-DM8168-APP-02 (RPS), DRAM: 1 GiB ( http://www.z3technology.com/Z3-DM8168-MOD.htm ) Software: EZSDK 5.02.00.57 : ( http://software-dl.ti.com/dsps/dsps_public_sw/ezsdk/5_02_00_57/index_FDS.html ) The aim of our...
    on Sep 12, 2011
  • Forum Post: Hang-up issue loading dm816x_hdvpss.xem3 firmware

    David Soto David Soto
    Hi All, I'm working with the following hw and sw components: Hardware: Z3-DM8168-APP-02 (RPS), DRAM: 1 GiB ( http://www.z3technology.com/Z3-DM8168-MOD.htm ) Software: EZSDK 5.02.00.57 : ( http://software-dl.ti.com/dsps/dsps_public_sw/ezsdk/5_02_00_57/index_FDS.html ) Problem: I have...
    on Sep 2, 2011
  • Forum Post: HDVPSS video decoder control migration from M3 to A8.

    Juan Solis Juan Solis
    Hello, I was wondering if anyone from TI can narrow down the time frame of when during Q4'11 the migration of the HDVPSS video decoder control firmware will move from the M3 to the A8. We have some early spins of some custom boards using the DM8168 but our H/W team was not aware that...
    on Sep 23, 2011
  • Forum Post: OpenMax and framebuffer simultaneous usage

    Piotr Ziecik Piotr Ziecik
    Hello. It is possible to use linux framebuffer together with OpenMax application ? I would like to have user interface on top of video, however I am not able to load vpss kernel module after starting OMX application (I am using SDK 5.00.00.11). Regards, Piotr Zięcik.
    on Aug 23, 2011
  • Forum Post: omtb customization

    Xianghua Xiao69249 Xianghua Xiao69249
    is there a omtb script or c-based app that can do: capture-encode-decode-scale-display? the existing omtb does capture-dei-encode-file and file-decode-scale-display separately, I want to bypass the sdcard/file operations. I'm also looking into vc3 demo(c-based), I think what vc3 does is : capture...
    on Oct 9, 2011
  • Forum Post: Video Input Capture: Is an "interlaced" resolution capture possible with EZSDK 5.02?

    Juan Solis Juan Solis
    Hello, Using SDK 5.02 I've been experimenting with non 1080p/720p resolutions for the capture_encode_a8host_debug.xv5T application. Using our custom boards and our own video decoder we've been able to "feed" the 8168's video input port's with other "progressive"...
    on Oct 12, 2011
  • Forum Post: Re: How to configure HDMI input port for OpenMax encoder component using DM8168 expansion IO Daughter board

    David Soto David Soto
    Hi guys, Is there any advance on this topic? I need to capture from the HDMI input as well, but according with the OMX documentation there are just two options for eHwPortId: OMX_VIDEO_CaptureHWPortVIP1_PORTA (J5, J6, J7 in daughter board) OMX_VIDEO_CaptureHWPortVIP2_PORTA (J2, J3, J4 in daughter...
    on Oct 24, 2011
  • Forum Post: Second frame buffer issue

    Jared Falter Jared Falter
    When ever I try echo 1 > /sys/devices/platform/vpss/graphics1/enabled I get: VPSS_GRPX : please open fb1 node first. I guess I don't know how to "open fb1" Here is the steps I am taking to get to this point. insmod /home/root/gpu/syslink.ko sleep 1 /home/root/gpu/slaveloader...
    on Oct 28, 2011
  • Forum Post: EZSDK 5.02 Memory Map

    Syoichi KONDO Syoichi KONDO
    Hi, How can I reconfigure the memory map of the ezsdk_5_02_01_59? The memory map is reconfigurable according to the Release Notes. I am trying to get the VPSS-M3 and VIDEO-M3 running in a 512MB memory. Regards, Shoichi Kondo
    on Sep 1, 2011
  • Forum Post: Why the system is crash?

    sheng zhou sheng zhou
    I use the hardware are "816X/389X EVM ASSY 512870 REV F" and "DM816X VIDEO SECURITY BOARD ASSY 513500 REV B" , the software i used is "DVRRDK_01.06.00.11", I change the "Rules.make" as this: ifeq ($(DVR_RDK_BOARD_TYPE ), ) DVR_RDK_BOARD_TYPE := DM816X_EVM endif...
    on Nov 11, 2011
  • Forum Post: Captured video images are offset to the right with EZSDK 5.03

    Claude Dansereau Claude Dansereau
    Hi, No matter if I am running the capture_encode example or my own GStreamer plugin, when I capture 720p60 video from the component input port, the images get offset to the right, and there is a small horizontal green band at the bottom of the images. This is happening with the latest 5.03 EZSDK,...
    on Nov 17, 2011
  • Forum Post: Re: VPSS in ezsdk5.03

    Robin Aproskie Robin Aproskie
    Hi Yihe I am using EZSDK 5.03 usinf the DM816 EVM and have downloaded the patch2 for V4L capture which has the new ti816x_hdvpss.xem3 firmware. Q1. Do I need to Load both the HDVPSS and HDVICP using firmware loader first and then additionally use slaveloader to load the ti816x_hdvpss.xem3 or does...
    on Dec 6, 2011
  • Forum Post: Re: dm8168 DVRRDK_01.06.00.11 deinterlace scaler

    Yaming Deng Yaming Deng
    Thanks for your reply Anshuman. Anshuman: I am not sure on how you got this inference. We use the links api as following: We exchange the encoder codec, and found that queue[DEI_LINK_OUT_QUE_DEI_SC] also can not upto D1. If the scaler is OK, did the nsf have the limition for the resolution...
    on Dec 12, 2011
  • Forum Post: dm8168 DVRRDK_01.06.00.11 deinterlace scaler

    Yaming Deng Yaming Deng
    We want run dual streaming on dm8168. We use deinterlace H and it can output 2 queues(DEI_LINK_OUT_QUE_DEI_SC and DEI_LINK_OUT_QUE_VIP_SC). But we found the queue[DEI_LINK_OUT_QUE_VIP_S] can scale upto D1 but the queue[DEI_LINK_OUT_QUE_DEI_SC] just upto 4CIF. Our problems: (1) Whether dm8168 deinterlace...
    on Dec 8, 2011
  • Forum Post: Do you have a plan for EzSDK support bayer format or other Image Sensor?

    RY9983 RY9983
    Do you have a plan for EzSDK support bayer format or other Image Sensor? Hello, I would like to directly capture Image Sensor in Netra HDVPSS. Do you have a plan for EzSDK support bayer format or other Image Sensor? Best regards, RY
    on Dec 13, 2011
  • Forum Post: Re: insmod vpss.ko hangs

    Carl Blake Carl Blake
    Aha, new load-hd-firmware shell scripts. I didn't see that before. One question, if we use the v4l2 script do we still need to change the notifyk.vpssm3_sva bootarg from 0xbf900000 to 0xa0000000 or should we keep it set to 0xbf900000? Carl
    on Dec 16, 2011
  • Forum Post: Not getting chroma conversion callback events with ezsdk_5_03_01_15

    sweta bhatt sweta bhatt
    Hi, We are able to run decode-display application from android rowboat project for DM8168. As per our understanding, TI components in this Android release are taken from ezsdk_5_02. Since we need to have V4L2 based video capture in Android, we planned to port ezsdk_5_03_01_15 release components...
    on Dec 31, 2011
  • Forum Post: The issue of setting MJPEG resolution dynamically base on RDK 01.08.00.15

    Yaming Deng Yaming Deng
    We set the resolution for MJPEG dynamically, but it seems have issue. As the picture shown, We use link api “DEI_LINK_CMD_SET_OUTPUTRESOLUTION” to set MJPEG as CIF and but the JPEG seems as D1. And H264 do not have this issue. We want know: (1) Is it the issue in MJPEG codec under...
    on Dec 21, 2011
  • Forum Post: Rebuilding The hdvpss and hdvicp m3 executables from source in EZSDK 5.02

    BenM BenM
    Hello, I have been provided the HDVPSS 1.0.1.28 source under NDA and can rebuild the examples. However, it would appear that none of the executables generated are the media controller executables provided in the target filesystem located at ~targetFS/usr/share/ti/ti-media-controller-utils. I would...
    on Dec 20, 2011
  • Forum Post: Utility to program EDID data of EEPROM (VC daughter card)

    sweta bhatt sweta bhatt
    Hi, Is there any utility to program EDID data of SII9135 ? We need to modify the default pre-programmed EDID data to support a specific capture requirement of a camcorder. Thanks in advance, Sweta
    on Jan 30, 2012
  • Forum Post: VC daughter card + HDVPSS - SII9135 doesn't function correctly for AUTO resolution of camcorders

    sweta bhatt sweta bhatt
    Hi, I plan to use JVCGZHD40TV (JVC camcorder) with VC daughter card's SII9135 HDMI receiver chip. There are only 3 resolutions supported by this camcorder (AUTO1, AUTO2 and 480p). When I use AUTO1 or AUTO2 mode with the camcorder connected to standard HDTV over HDMI, the HD TV(s) always detect...
    on Jan 30, 2012
12
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use