Warning message while communicating DM6437 EVM with PC through Host application

Hi!

          I am barani. I am working with DM6437 EVM. I tried to run the Host-Side demo application batch file. I connected the EVM board to the PC thorugh a router. When i selected the discover button, the EVM board's IP address and MAC are getting displayed.

         When i give Connect, the status bar displays as Connected, Playing. But when i see the java script window at the same time it displays a warning message as follows,

Main.js> warning: failed to read target statistics. Reason: JavaException: java.net.Socket Exception: connection rest by peer: socket wire error.

I am not getting any messages under Target messages area as displayed in Getting started guide page no- 3-7.

The DVDSK version i am using is dvdsk_1_01_00_15.  The host side appilication version is v0.51.00.

Why the java script showing this message. Kindly help in this case. I am unable to proceed with the application.

Regards,

Barani.