Hello,
I have a question regarding alsasrc used on a dm6467.
I have a pipeline that capture audio using mcasp (RX_MODE), encode and stream it over the ner (RTP).
I'm observing that it works ok if I set provide-clock=false as alsasrc parameter.
Not good if I set provide-clock=true.
What does it mean?
another question:
I'm using MCASP0 in RX_MODE with 2 serializer.
I receive AHCLKR from an external clock (that is clocked with the video clock), to avoid audio-video unsync.
But I don't uderstand how to have 2 input video in sync with the audio if the audio clock of mcasp0 is only one!
Thanks,
regards