• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » DaVinci™ Video Processors » DM64x DaVinci Video Processor Forum » Loosing the plot on DMA
Share
DaVinci™ Video Processors
  • Forums
  • Announcements
Options
  • Subscribe via RSS

Loosing the plot on DMA

Loosing the plot on DMA

This question is not answered
Chris Thomas
Posted by Chris Thomas
on Apr 21 2012 17:55 PM
Expert1020 points

I am wrestling with a system that is supposed to use DMA to get data from an FPGA.

The FPGA raises a line when it has a packet to read, it automatically drops the line as the last byte of data is read out (about 3 us), if there is another packet available it raises the line again (with a miniumum low period of 120 ns). The FPGA has up to 32 packets which it can transfer in quick succession.

To deal with this I have a essentially a ping pong setup (eg http://www.ti.com/lit/an/spra636a/spra636a.pdf  fig 28), the base channel is associated with a GPIO IRQ event, this channel is linked to 32 channels in a ring buffer. EDMA is setup to send me intermediate and final transfer completion callbacks.

I can see with a logic analyzer that the DMA controller has no trouble responding to the GPIO event and reading from the FPGA.

In a perfect world I would like to get a callback for every transfer, and in the parameters of the callback function, confirmation of which buffer has just been written.

In reality I find that I get few DMA completion events when there is a burst of DMA transfers, I can understand this, a string of IRQs can cause missed IRQs.

To counter this I made a non-nested, re-entrant, non-self-masking IRQ handler to catch the end of the transfer that simply increments a counting semaphore. By also toggling a GPIO pin I can see that these IRQs seem not to miss any transfers, but of course I cannot guarantee that.

I used the couting semaphore to control polled reading of the buffers but still seemed to miss some packets.

So I have gone back to the pretty unsatisfactory mechanism of writing a known pattern to the buffer before handing it to the DMA controller, and then checking for when the pattern is overwritten to know DMA has done its work and I can read the buffer and resote the know pattern (The buffers are in L1Data so there are no cache coherency issues to mess this up).

I expect to have a wave of written buffers to flow around the circular buffer for my polling routine to follow.

Even this does not work, I find that the buffers seem to complete out of order, that is I can be at position A checking the buffer, but due to counting IRQs and DMA completion callbacks I know there have been completions, in this case I peek at the next buffer and sometime find it has been written even thought the preceeding buffer has still not been written.

So am I missing the point, should this work, can this work, is there a better way?

Or on a simpler level, is thare an easy way to know what has just completed, and where data was just written, if nothing else, is there a way to read a count of completions from the DMA controller?

I just hate looking at a buffer and waiting for it to change underneath me, there are just too many ways for caching and optimization to confuse the issue.

Has anyone else implemented something like this and had success - just to give me some hope.

Chris

DMA EDMA 6433
Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Chris Bowers
    Posted by Chris Bowers
    on Apr 24 2012 09:45 AM
    Expert3330 points

    It seems that the DMA always works and the transfers are always complete. I suspect that the interrupts from DMA at the end of every packet are running into one another and do not meet the real time requirements. From my understanding of your system it would be better to devise a scheme that interrupted the CPU at the end of the up to 32 packet transfer rather than at the end of every packet.

    Chris

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Chris Thomas
    Posted by Chris Thomas
    on Apr 24 2012 12:15 PM
    Expert1020 points

    Hi Chris,

    I took your advice and removed the IRQs I can, now I have a task polling the buffers written to by the DMA controller which wakes up quite often (semaphore timeout), and also gets a poke from the DMA completion IRQ (posting the semaphore).

    I took out the piece of code that was polling the next DMA transfer address in the param block and went back to just seeing when the buffer has been written.

    I will test more overnight but so far it seems to behave much as before, with a little more latency processing isolated packets, and it still all goes wrong after a couple of million packets.

    Chris

     

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Chris Bowers
    Posted by Chris Bowers
    on Apr 25 2012 07:34 AM
    Expert3330 points

    Chris, can you confirm that the DMA always transfers the data correctly into the buffers? Is it just that picking up the buffers is still an issue?

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Chris Thomas
    Posted by Chris Thomas
    on Apr 25 2012 08:50 AM
    Expert1020 points

    Hi Chris

    I can confirm it always runs and reads bytes over emif, whether they get to the L1data is not something I can guarantee.

    My new plan is to get rid of most of the IRQs and use handshaking with the FPGA so it can spoon feed data to the DSP with no possibility of an IRQ that the DSP is not ready for.

    This will add latency I am sure, but with enough complexity the raw speed should be similar to the original design. In this new design there will be a per packet IRQ to the DMA controller, no completion IRQ from the DMA controller and a single IRQ to the DSP from the FPGA (which just increments a semaphore).

    A task will pick up the semaphore, do the read(s) and handshake back to the FPGA when it is done.

    Does that sound more achievable?

    The main problem I can see is if there is a significant delay between the DMA controller reading the data and it writing it to L1data, do you think I need to get the FPGA to put in some delay to allow for this? I was thinking that the IRQ latency and the subsequent delay until the task responds to the semaphore would be far greater than any write delay in the DMA controller - but if I am being optimistic please tell me.

    Chris

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use