Hi,
I am working on a boot loader for DM6437. The idea is to create 2 independent firmware that one will update another. In firmware1 i will download firmware2 file and write it to NOR flash in a specified address .Both firmware is stored in NOR flash in ais format. Now i have in flash two applications. one is my Custom boot loader and the second one is my main project. i want to know how can i jump from the first program to the second program located in a specified address. I also expect information about documents which helps to create custom bootloader
If someone can help me to jump it will be great.
Thanks