Hi,
I'm trying to add an opencv application code into /dvsdk_2_00_00_22\codec_engine_2_23_01\examples\ti\sdo\ce\examples\apps\video_copy\dualcpu\evmDM6446. This code was compiled and tested in CCS in ARM side. It runs ok for function test. Now the code was added into Linux and but got compile error as below:
I added the -lm compile option in makefile and compile. It shows
arm_v5t_le-gcc: -lm: linker input file unused because linking not done
and also same error.
My understanding is it need to use standard C math lib and -lm is to link the lib but it failed. Could anyone can tell me what the reason is? Thanks in advance!