Hello Everyone,
We are using TMS320DM6446 as our DSP processor and we are using XDS200 Emulator with TI14 pin connector on board and we have used adapter from CTI20 pin to TI14 pin, we are getting these errors respectively before and after powering on the board.
ERROR:
--------------------------------------------------------
Befor Powering ON
-------------------------------------------------------
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\RJK2015\AppData\Local\TEXASI~1\
CCS\ti\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'xds2xxu.out'.
The library build date was 'Oct 17 2014'.
The library build time was '22:03:24'.
The library package version is '5.1.600.0'.
The library component version is '35.34.40.0'.
The controller does not use a programmable FPGA.
An error occurred while hard opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-180' (0xffffff4c).
The title is 'SC_ERR_CTL_NO_TRG_POWER'.
The explanation is:
The controller has detected a target power loss.
The user must turn-on or connect the power supply for the target.
[End]
--------------------------------------------------
After Powering ON
--------------------------------------------------
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\RJK2015\AppData\Local\TEXASI~1\
CCS\ti\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'xds2xxu.out'.
The library build date was 'Oct 17 2014'.
The library build time was '22:03:24'.
The library package version is '5.1.600.0'.
The library component version is '35.34.40.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '13' (0x0000000d).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
This emulator does not create a reset log-file.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.
The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.
[End]
-----------------------------------------------------------
please anyone could help us on fixing this error.
Regards
J.K.Ranjan
Hardware Engineer