Hello,
I want to use GPIO[0:7] on dm648 board. According to the manual, I set the UHPIEN pin as high through a switch (verified by BOOTCFG bit17), and open the GPIO lpsc. When I write data to the GPIO registers(DIR01,OUT_DATA01), I see that all the registers become 0x00000000, and cannot be written. When I set the UHPIEN pin as low, the GPIO registers can be written, but the GP[7:0](configured as output) read from IN_DATA01 are always 0xFF.
Can anyone help me understand what is going on here?
Thanks,
Joshua