Dear all,
Hi, I am quite new to this forum, and hence a newbie. I have bought and now using TMS320DM6446 EVM, and my team is now developing through an emulator using CCStudio 5.3.
I have a question related to program code addresses. I need to know (or configure if possible) the exact program code addresses in order to:
1. Copy the program codes into Flash and then (restart and) boot the ARM from there
2. Enter the interrupt routine by setting the interrupt entry base address (the EABASE and IRQENTRY registers)
3. Copy part of the program codes into DDR so that I can boot the DSP from there
The problem is:
1. I don't know how to configure the program code addresses. Is it related to something like "#pragma"?
2. If I just read the addresses from the disassembly code after compiling, then whenever the program is changed, the addresses will change as well.
My question is:
1. Is my logic correct? Is configuring the program code address the correct way to do the above 3 things?
2. How to configure the addresses? I am using C. If necessary I can use assembly code.
I read through some of the related posts, but I have not found a solution. Any help will be greatly appreciated. Thank you in advance.
Regards,
AL