i WANT to implement interrupt based read write to/from MCBSP on c64+ core of dm6446 without using DSP/BIOS.Can anyone provide a c/psuedo code for it
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
i WANT to implement interrupt based read write to/from MCBSP on c64+ core of dm6446 without using DSP/BIOS.Can anyone provide a c/psuedo code for it
Hi Akash,
Thanks for your post.
I think, you can start with an app. report using c6000 McBSP for McBSP register configuration as well, you will find sample codes for McBSP in both master and slave mode in App. A and App. B from the app. report below:
http://www.ti.com/lit/an/spra455a/spra455a.pdf
To program the c6000 McBSP using CSL, there is a c6000 integration workshop for McBSP below in which there are paper exercise to write a sample code, kindly check the link below:
http://ext02.fh-kaernten.at/rts/intern/downloads/DSP/iw6000%20Chapter%206.pdf
Thanks & regards,
Sivaraj K
----------------------------------------------------------------------------------------------------------------
Please click the "Verify Answer" button on this post if it answers your question.
----------------------------------------------------------------------------------------------------------------
Hi Akash,
Thanks for your update.
We do have example code for timer in starterware as well CSL packages.
http://processors.wiki.ti.com/index.php/StarterWare_01.20.01.01_User_Guide#Example_Configuration
http://software-dl.ti.com/dsps/dsps_public_sw/c6000/starterware/01_20_04_01/index_FDS.html
Refer below wiki link for configuring GPIO Interrupt
http://processors.wiki.ti.com/index.php/Configuring_GPIO_Interrupts
if you need more information about interrupt registers and event combiner, refer below links
http://processors.wiki.ti.com/index.php/Setting_up_interrupts_in_DSP_BIOS
There are also CSL package available and also there is BSL based led blinking example and other sample code for DSK6713, please refer the below e2e post in which you can refer the attached 4628.dsk6713.zip file
https://e2e.ti.com/support/dsp/tms320c6000_high_performance_dsps/f/115/p/410542/1455896#1455896
Also, there is LED blinking example on omapl138 lcdk on the below e2e post, please refer the attached 4300.lcdk_led_echoApp_changes_SW1_10_03_03.zip
https://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/200324
Thanks & regards,
Sivaraj K
----------------------------------------------------------------------------------------------------------------
Please click the "Verify Answer" button on this post if it answers your question.
----------------------------------------------------------------------------------------------------------------