Hello.
I am currently cracking on a DM648 with the goal of establishing a secure ethernet point-to-point connection with the PC to provide a fast data transmission channel for downloading image frames right in the middle of the DSP processing them (at various stages). I'm trying to make the 3psw work properly, and I kind of fail.
I am bypassing the NDK, building it all from scratch. Everything up until now was more or less straightforward, but now I'm stuck figuring out the right way to tackle the ALE. My problem is, the DSP seems to accept all the packets being sent to it (mostly broadcast) without filtering anything. I need it to accept only a handful. However, as I try to configure the table, I always end up with the packets I need being discarded and the broadcast ones passing through. Can you please give me some ideas about the correct sequence of steps that get the ALE working the way it is supposed to? If there's an appnote or something similar, I would appreciate it tremendously if you could provide a link.
Thank you in advance