Hello,
As per the Transmit Buffer Descriptor Format mentioned in SPRUF57B, the PACKET_LENGTH is 11 bits and so i assume it should take a value up to 2047. But when i try to increase the packet length beyond 1518 bytes (including headers), i don't see any Ethernet packets transmitted from DM648. Could you please tell me why this happens? I am using Wireshark to capture the packets..
SP