Hi all ~
The function "VLIB_ORB_getHarrisScore" provided in VLIB has a parameter [const CORBInput input] , which is a struct defined as
CORBPatterns | patterns |
CORBOrientationOffsets | offsets |
uint8_t * | image |
uint8_t * | prefimage |
int16_t * | harrisImage |
uint32_t * | integralImage |
char * | scratchBuffer |
int8_t * | orbPattern31 |
My question is:
what is the last item [int8_t *orbPattern31]
No explaination is listed in all docs of VLIB~~~