HI,
I am trying to download a simple Application code (.bin) to flash (Say nor flash) in CCS v 5, currently it is downloading into DDR2 of my EVM.
Procedure i followed to create .bin file is mentioned in the below link.
e2e.ti.com/.../1296486
e2e.ti.com/.../1520251
For porting the .bin file we follwed instructions mentioned in the link
processors.wiki.ti.com/.../Serial_Boot_and_Flash_Loading_Utility
Switch Config is SW3-1 is(1), SW3-2 is (0) that is [1010111111]
-stack 0x00000800 /* Stack Size */
-heap 0x00000800 /* Heap Size */
MEMORY
{
IRAM: o = 0x00000000 l = 0x00004000
DRAM: o = 0x00008000 l = 0x00004000
AEMIF: o = 0x02000000 l = 0x02000000
DDR2: o = 0x80000000 l = 0x10000000
}
SECTIONS
{
.bss > AEMIF
.cinit > AEMIF
.cio > AEMIF
.const > AEMIF
.stack > AEMIF
.sysmem > AEMIF
.text > AEMIF
.ddr2 > AEMIF
}
and ran:
sfh_DM644x.exe -norerase and
sfh_DM644x.exe -norflash_noubl led.bin
still no improve. same log as mentioned in previous update.
If I change switch config to NOR boot and run in hyper terminal I get below LOG, but no lED glowing
U-Boot 1.1.3 (Mar 3 2006 - 01:16:59)
U-Boot code: 81080000 -> 810973A8 BSS: -> 810A02B8
RAM Configuration:
Bank #0: 80000000 256 MB
unknown vendor=89 Flash: 0 kB
*** Warning - bad CRC, using default environment
In: serial
Out: serial
Err: serial
ARM Clock :- 283MZ
DDR Clock :- 189MZ
Hit any key to stop autoboot: 0
BOOTP broadcast 1
WARN: emac_send_packet: No link
BOOTP broadcast 2
WARN: emac_send_packet: No link
BOOTP broadcast 3
WARN: emac_send_packet: No link
BOOTP broadcast 4
WARN: emac_send_packet: No link
BOOTP broadcast 5
WARN: emac_send_packet: No link
BOOTP broadcast 6
WARN: emac_send_packet: No link
BOOTP broadcast 7
WARN: emac_send_packet: No link
BOOTP broadcast 8
WARN: emac_send_packet: No link
BOOTP broadcast 9
WARN: emac_send_packet: No link
BOOTP broadcast 10
WARN: emac_send_packet: No link
Retry count exceeded; starting again
azhagiri