Hi,
I am working on DM6446 DSP, but sometimes after execution it goes out of its memory.
When i checked its registers status, i observed following things
- TSR shows interrupt blocked bit set to 1, interrupt execution bit set to 1
- IFR shows its 5 and 6 bit set to 1
- IER and IEER register both having value zero.
So from this i believe is it something to do with interrupt handling as it shows two interrupt bits set or is it normal for DSP to latch two interrupts bits.
Please guide if dsp can go out from its memory range from some other issue also.
Regards