Use DM6437 chip.Software environment is dvsdk. The board is used for human tracking .Basic reference design is mainly used.
The problem is that the video output should be in color, but actually it is black and white. Experiment named color bar is done for the test. The principle of it is DSP VPBE display color bars directly and then sent. And basically the program is no problem , but the result is still stay black and white . Further testing, DSP DAC output is just black and white. The figure below is the analog waveform measured.
To contrast ,I had colorful colorbar waveform on other's board, substantially the same with me, below is another good colorful colorbar graphics . Because of the high precision for analog video signal , time is in 'us' level, so my wave ripple though is small, but relatively worse than others, I do not know whether my ripple waveform is relatively too large and there should be a straight line but mine has a little rise.Difference can be seen from the chart.
I set the output format to pal, display screen standard mode is optional, the selection is of course pal. In addition, the same board was done for two pieces, one of which is off after a very long time, and then when the power is on ,it displayed in color, but the color is very poor, then it becomes black and white again. The other one is always black and white .
What causes problems above? Does layout cause? Whether there are some layout rules about analog video output ?Whether there are some related instruction manual?Please answer me! Thanks . PS:my Eglish is not very good ,if there are any grammar probloms,please acknowledge.thanks again!