Dear Support :
I tryed nand flash boot use colorbar program. It's work fine. [ perl version 5.14.2 ]
Same steps try to use video_preview, but fail.
Check BOOTCMPLT reg (0x01c4000c) got ERR_BAD_CRC error value.( 0x4 )
Try disable CRC Check :
genAIS.pl -i video_preview.out -o video_preview.bin -otype bin -bootmode nand -crc 0
write image to NAND flash and reboot target board. but cannot bootup. BOOTCMPLT reg is 0x0.
try to :
1. open CCSv3.3
2. only load gel file (evmdm6437.gel) in CCS and connect to target
3. Click Debug menu "Run Free"(Ctrl+F5) and "Reset CPU"(Ctrl+R) button.
4. video_preview start run on target board.
Please give me suggestion.
Thanks.
B.R.
Allen