1.STATE:before using network transmission, we can processing at 60 frames per second in local development environment(DM648 evm) For a video processing projects;But after we add the network transmission by the NDK 2.0, we can only processing at 15 frames per second.
2.Survey: we find the DSP core(DM648) is always busy when the network transmissing.so the Frame rate reduce.
3. PLATFORM: DM648, CCS4.2, DSP/BIOS 5.4.1, NDK2.0
QUESTION: How to reduce the CPU consume produced by NDK 2.0?
ie.EMDA3,can we use the EMDA3 to transfer the data block to NETWORK MODULE,instead of using the DSP core.