Hi,
I have a question about DM6446 USB PHY initialization.
At the end of USB PHY initialization when setting USBPHY_CTL.PHYPDWN bit
from 1(powerd off) to 0(powered on), USB_DP and USB_DM voltage goes to about 1[V] for a moment
and then drop to about 100[mV]. Pleas see the atached file which I capture the signal from oscilloscope.
Is this a specification of DM6446 USB?
And will this affect to USB enumeration and data communication?
This issue are seen at DM6446EVM and my customer's board.
best regards,
g.f.