Hi ,
When I use the function VLIB_houghLineFromList() in vlib for Hough Transform, I have a question:
First, I do not konwn what are the parameters " ping pong pang peng" mean?
Second, when I get the parameter "pOutHoughSpace" from VLIB_houghLineFromList() , and I get the biggest pixels index in "pOutHoughSpace", for example 200, and I suppose the thetaRange is 180, rhoMaxLength is 267. How can i get the true Theta and Rho? Theta = 200 / rhoMaxLength , Rho = 200 % rhoMaxLength ? What is the relation between the input parameter rhoMaxLength and the Rho/Theta?
Thanks a lot.