Hi
I use acpy functions to transfer 1920×540
byte to the second half of frame but in this case all of the frame is distorted and jumped;what is the problems ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I use acpy functions to transfer 1920×540
byte to the second half of frame but in this case all of the frame is distorted and jumped;what is the problems ?
Hi,
Thanks for your post.
We do have any source code for ACPY2, which you could use for re-building the library. Please find attached the zip file for ACPY2 source code below:
/cfs-file/__key/communityserver-discussions-components-files/791/1588.1616.spra789a.zip
Section3 describes the C6x1x-specific (C6211, C6711) ACPY2 implementation provided with the application note below:
http://www.ti.com/lit/an/spra789a/spra789a.pdf
Thanks & regards,
Sivaraj K
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question
-------------------------------------------------------------------------------------------------------
I use acpy3 library and it work for small memory for larger transfer that I was explane later it not work properly