Hi,
Please suggest me good processor for 3d image processing (adaptive filtering ) and camera support application.
Thanks in advance,
Ravishankarkm
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Please suggest me good processor for 3d image processing (adaptive filtering ) and camera support application.
Thanks in advance,
Ravishankarkm
Hi,
Thanks for your post.
In my understanding, TMS320DM6467T, a new DaVinci video processor designed to meet the demand for increased digital video quality, higher resolution and faster frame rates for video communications and security applications. The 1 GHz DM6467T is a single-chip processor that enables networked digital video applications to decode high-definition (HD) H.264 (1080p at 60 frames per second (fps)).
Key features:
The combined performance of a 1 GHz C64x+(TM) DSP and 500 MHz
ARM926EJ-S
-- Supports H.264 1080p decoding up to 60 fps, a well as eight
simultaneous channels of H.264 D1 real-time video encoding with
solution from a third party
-- Higher core speed with flexible DSP programmability provides
sufficient processing capacity to implement advanced video processing
algorithms and functions
-- Faster DDR2 interface at 400 MHz facilitates higher bandwidth for more efficient video throughput
-- Two integrated 500 MHz High Definition Video/Imaging Co-Processors
(HD-VICP) accelerate video processing and increase application
efficiency
-- Faster 150 MHz video port interface supports 1080p capture
For more info. kindly refer the below links:
http://www.dm6467t.com/evm/#dm6467tevmspecifications-1
http://www.dm6467t.com/files/DM6467-EVM-TI-DaVinci-High-Definition-Evaluation-Module.pdf
Thanks & regards,
Sivaraj K
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question
-------------------------------------------------------------------------------------------------------