I am working on a project with a monchrome CMOS sensor attached to a DM6435. Much of the video material is based upon color sensors. Two items have come up as particular questions:
1. Document SPRU977A section 4.3.1.2.3 pages 41-42 discuss the Fault Pixel Correction. We are using a 12 bit monochrome CMOS imager. The first descriptions of the correction mechanisms state that the pixel corrections are done with pixels “of the same color”. Is the system capable of doing this correction for us or is it going to assume a Bayer pattern? We just want to use the adjacent pixel. Table 17 does not have this qualifier “of the same color” so it occurs to me that the system may not know the color pattern of the sensor and method 0 will really do what I want.
2. The Preview Engine does dark frame subtraction which we want. Unfortunately, it forces RGB blending and RGB to YCbCr conversion. Are there settings that will allow us to nullify the effect of those stages or are we better off doing the subtraction with the processor?