Other Parts Discussed in Thread: MAX3232
Tool/software: Code Composer Studio
hi,
My DM6437ZWT core board,when running NDK program at full speed(CPU@594MHz,DDR@162MHz), the temperature of the case surface is 62 ℃。(Ambient temperature is 27 ℃)
Then ,I disassemble the other IC, only keep the power, reset IC,MAX3232 and CPU,use this minimal systems running a led slash program(Use UART BOOT mode download). The temprature of the case surface is 49℃.
Is this normal?
Do I need to add a heat sink for CPU?
Thanks