Hi All,
I would like to ask a question in SPRU977a, 643x VPFE document, page 91:
In the previous page (p. 90), the impact of VDLC value on SDR_ADDR (one of the shadow registers) are explained. This is clear and has no ambiguity.
However, on page 91, I don’t understand “CCDCFG.VDLC must be set to 1 by software if the CCD controller is to be used”. Does it sound that VDLC is the enabling register bit for CCDC? But even if I set VDLC to 0 and test it on the EVM, the VPFE still works and generates stable output to VPBE (and display).
I also cannot understand “If CCDCFG.VDLC remains cleared to 0 (default), indeterminate results may occur for any register access in the CCD controller, not just the following registers.”
What does
1. intermediate results
2. may occur
3. any register access
mean respectively?
Sincerely,
Zheng