Hello,
The Documentation is confusing to me so I've got to ask. I want to use the User Defined LEDs on my EVM board which are tied to GPIO2-GPIO5, but I'm not having any luck. I believe I am setting up the GPIO module correctly, however, I'm not sure about the PinMux Select Register. The instructions are unclear to me as to if the GPIO0-7 lines are even muxed or not (as shown in Table 3-8 in the tms320dm647 datasheet). Also, what does Table 3-7 mean with the Unmuxed or Muxed Columns? Is this the same as Primary and Secondary Functions of the Pins?
Thanks for any help.
--James Rasmussen