• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » DaVinci™ Video Processors
Share
DaVinci™ Video Processors
  • Forums
  • Announcements

Browse by Tags

DaVinci™ Video Processors

Welcome to the DaVinci™ Video Processors Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
1080P
  • 1 DM365 DM368 DM36x
  • 1 DM365 DM368 DM36x IPNC V4.0
  • 8127 ipnc
  • 8127 RDK
  • 8148
  • 8148evm
  • 8168
  • 8168 debug
  • 8168 dvr rdk
  • 8168 DVR_RDK
  • 8168 evm
  • 8168 EZSDK
  • 8168 ezsdk omx
  • 816x
  • 81xx
  • Appro
  • Da Vinci dm6467
  • DM365
  • DM368
  • DM3730
  • dm6437
  • DM6467
  • dm8168
  • DVSDK
  • V4L2
Related Posts
  • Forum Post: DM365 and 1080p @ 30pfs

    Y.Chay Y.Chay
    Hi, I need to translate CMOS sensor RAW data (Bayer) into BT.1120 or other standard parallel digital video format (CEA-861) with 1080p30 performance. My application does not require any CODEC. Can I use the DM365 to do the job? Thanks, Yossi
    on May 29, 2009
  • Forum Post: DM6467 VPIF

    Richard Hall Richard Hall
    Hello, I am working on a project where we want to take 1080p30 video out of an OmniVision OV5633 and encode it to h.264 with the DaVinci at 30fps fand transmit the h.264 data stream. All of on this project are new to any of this sort of work so we have no clu where to start with it. What we think we...
    on May 29, 2009
  • Forum Post: 1920x1080 H.264 encode demo on DM6467

    Douglas Reher Douglas Reher
    Hi, I'm a new user of the 6467 DVEVM. I've been trying to modify the "encode" demo that is included with the DVSDK to allow encoding of 1080 video. Simply changing the maxHeight and maxWidth parameters in the VIDENC1_Params struct is apparently insufficient, as the Venc1_create()...
    on Jun 24, 2009
  • Forum Post: Re: 1920x1080 H.264 encode demo on DM6467

    Doug Rogers Doug Rogers
    Bernie, thanks for the info about DVSDK 3.10 stabilizing for the plain 6467 over the coming months. I've been reading this thread hoping to discover as much as I can about 1080p30 support for the two 6467(T) DVEVM boards. The specs for the DVEVM for the T part indicate that its DVSDK contains...
    on Mar 11, 2010
  • Forum Post: Re: Does TIDM368SDK support capture raw data from V4L2 interface?

    Tan Rick Tan Rick
    Hi Anshuman, Thanks for your reply. But I have another question. Can DM368 support 2*1080P(<=15fps) + 1*CIF triple stream if we get video data via V4L2 interface? firstly , DM368 support 4 /dev/video? Sencond, Does DM368 codec can support this capacity? Thanks. Rick
    on Apr 13, 2011
  • Forum Post: How can full HD resolution(1920*1080@30fps) image input on DM3730

    Hyunho Shin Hyunho Shin
    Does anyone know how can input 1080p@30fps resolution from camera on DM3730? please advice me
    on Apr 19, 2012
  • Forum Post: RE: How to configure the drivers' parameters for DM648??

    maoyang wu maoyang wu
    Hi, why no answer to the question above? By the way, We can get Y data correctly, while the Cb and Cr data is wrong, why and how to solve it. Thank you! M.Y. Wu
    on Apr 24, 2012
  • Forum Post: Why DM368 DA pins can't output any signal ?

    op op op op
    Hi all~ I am sorry to be a DM368 novice. I want to decode a 1080P H264 file and output "Y\Pb\Pr" singals to the interface of color component through 3 DA pins of this chip. Demo programs located in the DVSDK (dvsdk_dm368-evm_4_02_00_06) are used to encode and decode this 1080P file after minor...
    on May 30, 2012
  • Forum Post: RE: raw capture on dm6437

    osunm osunm
    Hi, I saw another way to try . A . C hange to the size was 960x1080 to downsamplerate . PrevParams->downSampleRate = PSP_PREVIEWER_DOWN_SAMPLE_RATE2; B . Previewer of the output images were stored on DDR2 . A result of the Resizer (960x1080-> 640x480) is shown below . Still come out the wrong...
    on Jun 14, 2012
  • Forum Post: DM6437 occurs in raw capture

    osunm osunm
    Hi! I have the DM6437 will try to raw capture . The OV2715 (1920x1080) image sensor receives 1080p video. The CCDC is 1080p (1920x1080) video 720p (1280x720) makes a crop . The previewer to convert the raw images , it stored in SDRAM as YcbCr forma . My work is illustrated in the following...
    on Jun 20, 2012
  • Forum Post: RE: about DM365 IPNC hang up "DRV_isifWaitInt(DRV_ISIF_INT_VD0, 2);"

    ranjana kumari ranjana kumari
    i am using dm368 EUCDK on leopard board. can anyone suggest how can i get the ip address of the target board since ifconfig is not working.
    on Jul 18, 2012
  • Forum Post: How to redirect video feed from HDMI RX to HDMI TX

    shakthi pradeep shakthi pradeep
    Hi, We are planning to use DM8168 in our design which would be used to perform the following. 1) Our design with have one HMDI RX port and Two HDMI TX ports. Stream from HDMI RX has to be split into two halves and each half has to be sent over the two HDMI TX ports 2) Video from the HDMI RX port...
    on Jul 18, 2012
  • Forum Post: Can dm6467t h.264 encode 1080p60?

    changming sheng changming sheng
    hello It is possible to capture 1080p@60 frames from VPIF of dm6467T. i want to konw whether the encoder 1080p@60 frames is possible on dm6467t?
    on Jul 26, 2012
  • Forum Post: Can DM368 encode 1080P video of which the colorspace is UYUV?

    Bing Xu Bing Xu
    In the encode demo of DM368, only UV420PSEMI and 1080I is supported. I'm trying to encode 1080P video of which the colorspace is UYUV. however, it seems128MBytes (68MBytes for CMEM) is not enough for DM368 to do such a job. I guess it is because that UYUVY need 2 bytes for each pix, while UV420PSEMI...
    on Aug 10, 2012
  • Forum Post: Three video streams at 1080p60?

    MRI MRI
    How can you do three 1080p60 streams with two video input ports? If you split the ports to 8 bits, you can't do 1080p60 with an 8 bit bus at 165 MHz. Please explain?
    on Aug 31, 2012
  • Forum Post: RE: 816x Expansion I/O daughtercard: Which Inputs are supported by SDK?

    sadasivappa s sadasivappa s
    Hello HardikShah, I am working on DM816x-EVM(Netra) based custom board. Custom board setup is as following: We have DM816x Video ports connected to FPGA logic. At video RX side FPGA will recieve video from HD-SDI and converts it to 1080p30/1080p25/720p50 format and feed to VIN0 (x16) of DM816x...
    on Sep 12, 2012
  • Forum Post: gstreamer could not negotiate format for 1080p25 & 720p50

    sadasivappa s sadasivappa s
    Hello, I am working on DM816x-EVM(Netra) based custom board. Custom board setup is as following: We have DM816x Video ports connected to FPGA logic. At video RX side FPGA will recieve video from HD-SDI and converts it to 1080p30/1080p25/720p50 format and feed to VIN0 (x16) of DM816x. At video...
    on Sep 12, 2012
  • Forum Post: DM816x: H.264 decoder bit rate

    sweta bhatt sweta bhatt
    Hi, I wanted to know whether DM816x H.264 decoder is dependent of video bit rate parameter or not. I have a requirement as below 1) to decode 4 1080p/ 4 1080i encoded streams at 15 Mbps. Is there any constraint/limitation to support maximum bit rate for each HD channel? 2) to decode 16 SD resolutions...
    on Sep 28, 2012
  • Forum Post: RE: Capture video when incoming video resolution changes on the fly

    Michael Erdahl Michael Erdahl
    Tiebing, Please have a look at this: http://processors.wiki.ti.com/index.php/TI81XX_PSP_VIDEO_CAPTURE_Driver_User_Guide#Querying_DV_preset There is code there to query current input resolution detected by the decoder. You'll need to get the file descriptor of the input stream, /dev/video0...
    on Oct 1, 2012
  • Forum Post: How to Exit gracefully while omx didnot work normally?

    feng xiao ming feng xiao ming
    Plateform:DM8168+EZSDK5.05 I run the decode_display_a8host_debug.xv5T example,but it blocked,and cannot be killed by CTRL+C. How to solve this problem, let the omx examples Exit gracefully? root@dm816x-evm:/home# ./decode_display_a8host_debug.xv5T -i 1080P_HP.h264 -w 19 20 -h 1080 -f 60 -g 0 -d...
    on Nov 2, 2012
  • Forum Post: RE: DM368 IPNC with ov2710

    bonggyu Choi bonggyu Choi
    Renjith, I use 30fps 1080P mode. by the way, I think your first advice would be right. because it could be overwrite processing frame. so, I consider one more possibility of this issue. But, I don't understand OV2710 image sensor. it only output RGB raw data with CCIR656. I think CCIR656 only support...
    on Nov 21, 2012
  • Forum Post: RE: DM368 IPNC with ov2710

    bonggyu Choi bonggyu Choi
    Renjith, I got it. Could you let me know what I shall check? Is that enough to check your thread? BR, Choi
    on Nov 21, 2012
  • Forum Post: RE: DM814x by camera interface (port) with BT.1120 YUV input

    Jiger Ho1 Jiger Ho1
    Dear Margarita, OK, I involve Oddy to here to show the problems and our progress on the project,he is my colleague. thanks again. Jiger
    on Jan 9, 2013
  • Forum Post: RE: Integrate YUV sensor for IPNC App V2.6

    Jiger Ho1 Jiger Ho1
    Dear Bioz, We have same promblems.It seems Y/C components are sawapped.we are using 16bit YUV mode with IPNC3.2.Can you tell me how to solve it?thanks very much. JIiger
    on Jan 9, 2013
  • Forum Post: reliability of APPRO SDK for DM368

    bonggyu Choi bonggyu Choi
    Hi, I develop recording application with appro SDK for DM368 IPNC. capure resolution is 1920x1080P. I found that average frame capture time and frame rate vary with my recording application. Even though they are vary with some linux util as like TOP. Parameters only appro SDK(means run ony system_server...
    on Jan 23, 2013
12
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use