• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » DaVinci™ Video Processors
Share
DaVinci™ Video Processors
  • Forums
  • Announcements

Browse by Tags

DaVinci™ Video Processors

Welcome to the DaVinci™ Video Processors Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
1080i
  • 'DM8168
  • 1080p
  • 1080p h264
  • 1080p/30 encode
  • 2 VIP instances
  • 368
  • 8168
  • 8168 codec h263
  • 8168 codec h264
  • 8168 codec h264 runtime
  • 8168 codecs
  • 8168 dvr rdk
  • 8168 DVR_RDK
  • 816x hdvpss
  • capture
  • DaVinci DM368
  • DM365
  • DM368
  • dm8168
  • DM816x
  • Encoder
  • H.264
  • interlaced
  • omx
  • video
Related Posts
  • Forum Post: DM365 capture interlaced video from CCD without embedded sync

    Juraj Juraj
    I'm trying to start capture of interlaced (1080i) input video signal on EVM DM365 connected on the CCD port. Signal is synchronized using CCD-FIELD signal routed to C_WE_FIELD pin, VDIN_HD, VDIN_VD. It works.
    on Nov 12, 2009
  • Forum Post: DM368 maximum video out clock frequency

    Nara Won Nara Won
    After discussing with experts, following conclusion was gotten. The maximum video output clock frequency DM368 can handle is 75MHz. DM368 can get external video clock but it cannot handle faster than 75MHz. With 75MHz 1080p 30fps is possible. But LCD pannel requires 1080p 60fps. To get 1080p 60fps...
    on Jul 6, 2010
  • Forum Post: DM365 frame rate decimation from 30 Hz to 15 Hz

    JayVee JayVee
    Hi, we're using the DM365 processor to capture live 1080i video at 30 frames per second, but the DM365 is transmitting this video at 15 frames per second. We're trying to find out why the DM365 is decimating the frame rate. Here is what we know so far: The capture system is indeed capturing at...
    on Jul 21, 2010
  • Forum Post: h.264 encoder

    Al Carlson Al Carlson
    Normal 0 false false false EN-US X-NONE X-NONE MicrosoftInternetExplorer4 ...
    on Feb 8, 2011
  • Forum Post: DM8168 Problems with encode interlaced h264

    anthony convers anthony convers
    Hello, I'm working on DM8168 EVM platform, my EZSDK version is 5_03_01_15. I try to encode a 1080i60 stream on the SD card with the OMX application. I use encode example. I made some modification in file ilclient_utils.c to configure encoder for interlace encoding : I uncomment the part...
    on Apr 18, 2012
  • Forum Post: Capture problem in 1080i in DM8168

    George K George K
    We are seeing a problem with HDMI 1080i input capture on DM8168. The capture-encode demo code present in ezsdk_5_03_01_15 has been modified to just use the capture OMX component. The captured output is showing only one field correct and the other field being garbage. We are not using DEI or any other...
    on Jun 1, 2012
  • Forum Post: DM368 1080P@30fps decode net stream Issue

    Baijian Liao Baijian Liao
    Here we want to use dm368 to decode 1080P@30fps H.264 network stream,which is from network in MPEG2-TS format. But after doing some effort,we found that DM368 seemed to can only decode from .264 file,but not from network stream.When H.264 stream with bitrate @8Mbps, error normaly happen,expecially when...
    on Jun 5, 2012
  • Forum Post: DM368 HD video and AAC audio encoder performance issue

    Jason Dong Jason Dong
    Hi, I am trying to encode the HD video and audio at the same time on DM368 platform. The encode formats are H.264@1080I and AAC@48K sample rate. However, the video frame rate is below 29 fps with capture and encode only. Is there any way to improve the performance to encode HD video and audio...
    on Jun 21, 2012
  • Forum Post: Does DM816x support 6 channel 1080I_60 decoding ?

    sweta bhatt sweta bhatt
    Hi, I know that Netra supports up to 3 1080P_60 or 6 1080P_30 decoding (with 3 HDVICP cores). Can someone please confirm whether Netra can support 6 channel 1080i_60 or 3 channel 1080i_60 decoding ? Regards, Sweta
    on Sep 20, 2012
  • Forum Post: DM816x: H.264 decoder bit rate

    sweta bhatt sweta bhatt
    Hi, I wanted to know whether DM816x H.264 decoder is dependent of video bit rate parameter or not. I have a requirement as below 1) to decode 4 1080p/ 4 1080i encoded streams at 15 Mbps. Is there any constraint/limitation to support maximum bit rate for each HD channel? 2) to decode 16 SD resolutions...
    on Sep 28, 2012
  • Forum Post: How two change encode framerate?

    Mary long Mary long
    Hi,I use DVRRDK 03.00.00.00 for development. Hardware platform is EVM8168. My code is used for test encode performance. read raw data from files(interlace data) --> IpcFramesOutHLOS --> IpcFramesInVideoM3 -->Enc -->IpcBitsOutVideoM3 --> IpcBitsInHLOS --->save bits to files. however...
    on Jan 5, 2013
  • Forum Post: How can I do video overlay after encode from HD camera and then stream out to network using rtp

    baochang wang baochang wang
    Hi, I'm using the Z3-DM8168-RPS system, it can stream in from HD camera, and stream out by network using rtp, Is someboay can tell me how can I draw some graphics on the video before stream out? I tried many ways based on TI EZSDK. but i'm not sucess. please help. thanks
    on May 2, 2013
  • Forum Post: DVRRDK 4.0 Release time.

    Mary long Mary long
    Hello, DVRRDK 4.0 is released or no? IN http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/t/224828.aspx?pi239031349=2 , mentioned " RDK 4.0 will be available end of Apr."
    on May 10, 2013
  • Forum Post: Extending DM8168 1920x1080 (8bit) capabilities

    David Aviv David Aviv
    Hello, Following a previous conversation on this matter, I have understood that the DM8168 has an hardware limitation for video in (line length of 1920 bytes). Since I'm using an imaging sensor of 10 bits, which is extremely important for DSP purposes, I need to transfer line of 1920 of 10 bits...
    on May 20, 2013
  • Forum Post: DVR_RDK 4.0 encode Interlaced input chroma issues

    Robert Lancaster1 Robert Lancaster1
    We are having an issue encoding two interlaced inputs of differing resolutions on RDK 4.0 with the DM8168/9. If VIP0 has a 16-bit 480i30 input and VIP1 has a 16-bit 1080i30 input there are noticeable chroma errors in the encoder output: However, if both inputs are switched to be 1080i30 the encoder...
    on May 22, 2013
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use