• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » DaVinci™ Video Processors » All Tags » 1080p60
Share
DaVinci™ Video Processors
  • Forums
  • Announcements

Browse by Tags

DaVinci™ Video Processors

Welcome to the DaVinci™ Video Processors Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
1080p60
  • 04.04 release
  • 1080i60
  • 1080p
  • 1080p30
  • 1080x1920
  • 720p
  • 720p on DM385/DM8127
  • 8148
  • 8148 codec engine example hangs up
  • 8148 DDR3
  • 8148 iss vpss video image capture 814x ezsdk omx 8148 HDVPSS capture fvid2 814x hdvpss
  • 8148 mmc
  • 8148 rbg656 rbg666
  • 814x
  • 8168
  • 816x
  • 81xx
  • A8
  • AES Decryption on DM814x / DM81xx
  • Codec
  • DaVinci
  • dm8148
  • encode
  • HDVPSS
  • Video
Related Posts
  • Forum Post: TI8148EVM capture/encode/display 1080p60 vs 1080p30

    Andrea Scian Andrea Scian
    Dear All, I'm working with TI8148EVM and SDK 5.03.01.15 Our test bed is based on a 1080p60 source (which is our custom DM8148-based board) that play dm816x_1080p_demo.264 demo stream provided with the SDK root file system. On the other side I have TI8148EVM that takes this input (via...
    on Mar 28, 2012
  • Forum Post: Re: TI8148EVM capture/encode/display 1080p60 vs 1080p30

    Andrea Scian Andrea Scian
    I've done some more test on this.. When playing the captured h264 raw file on a PC (e.g. with VLC or mplayer) I see that it's at 25fps: [snip] Playing /mnt/naon/dm816x_1080p30_encode.h264. Invalid seek to negative position ffffffffffffffff! libavformat file format detected. [h264 @ 0xa2538a0...
    on Apr 3, 2012
  • Forum Post: RE: DDR3 512MB settings and video capture

    Jun_Zhang Jun_Zhang
    update: If I following the steps in the ezsdk_memory_map and set notifyk.vpssm3_sva=0xBF900000 and vpss sbufaddr=0xBFB00000 The error is gone. However, could any TI expert clarify this for me. If I am using 512MB DDR3, and I want to use v4l2 vpss firmware, I just need follow the steps in...
    on May 2, 2012
  • Forum Post: v4L2 capture related to 512MB DDR3 settings?

    Jun_Zhang Jun_Zhang
    Greetings, My board is based on dm8148 with 512MB ddr3 and now I am using ezsdk5.04/5.03. After applying the sub-device-call remove and select decoder patchs, my board can do certain video capture from our custom hdmi receiver. However, this is not stable at all. I am using v4l2 firmware and not...
    on May 2, 2012
  • Forum Post: Videostream manipulation

    Johannes N Johannes N
    Hello, i am quite new to DSP/ARM development. I have a Mistral EVM with DM8148 and display. We need to modify every pixel of a realtime 720p60 videostream (directly from sensor) with a logarhythmic function involving neightbour pixels. I cannot find a suitable starting point for integrating a modification...
    on May 14, 2012
  • Forum Post: Wheather Dm81xx can decode the H264 video with 25fps(not 30fps) ?

    zhichao tan60372 zhichao tan60372
    Hello all: Now I use ezsdk_5_04_00_11(or the older version) on DM8148,When I use the gstreamer command to play a H264 video with 25fps(not 30fps) ,I found the rate of playing the video was faster than the actual rate,although I set the framerate of the caps to 25fps,Accoroding to the file gstomx_h264dec...
    on May 30, 2012
  • Forum Post: V4L2 capture and VPSS features

    Karthik Kumar Karthik Kumar
    Hi, 1. Is V4L2 Capture supported in latest Netra EzSDK that is available? If yes, then 2. Does V4L2 exposes a method/interface to configure VPSS features like EDE (Edge Detail Enhancer) and DRN (De-Ringing) ? Please let us know your inputs on above points.
    on Jun 15, 2012
  • Forum Post: Reading EDID of display and programming o/p timing generation

    sweta bhatt sweta bhatt
    Hi, I have a query regarding HDMI Display. Is it possible to read the recommended frame rate out of the displays EDID and use this information for output timing generation ? If yes, any idea, how this can be achievable in DM816x ? Regards, Sweta
    on Sep 21, 2012
  • Forum Post: omtb 720p60 capture and display hangs

    Xing Yu Xing Yu
    Howdy all, I'm having an initial play with omtb .oms scripts using EZSDK 5.03.00.09. I am using a camera that cannot output 1080p60 but can do 720p60 so I am trying to modify the provided scripts to work with that. By combining a couple of provided scripts and also some posted on this forum, I...
    on Sep 21, 2012
  • Forum Post: 1080i60 support

    Ashwin Bihari Ashwin Bihari
    I have a custom board that is based around the DM8148 and has a TVP70025 (industrial temp version of the TVP7002 that's on the EVM) and I need to support HD video at 1080i60 on this board. I've tested 720p60 and 1080p60 and both work as expected. The saFbdevLoopback application has a comment...
    on Dec 19, 2012
  • Forum Post: DM8146 Video streaming via ethernet port

    DEV1 DEV1
    Hi, I'm looking to get started with programming in Linux for the DM8146. In particular video streaming and substreaming, where should I look for some open source libraries with documented API's. I'm interested in H.264 encoding and decoding, all via the ethernet port - I'm sure there's...
    on Apr 7, 2013
  • Forum Post: DM814x HSYNC & VSYNC Polarity

    Danny Cullen Danny Cullen
    Dear all, I am using a custmo Dm814x board and can capture using V4L2. My input is a 1920x1080p60 24-bit RGB source with discrete syncs. I capture the image below which is ok for 720 lines and then possibly then start of the next frame has been DMA'd into my buffer. I've checked and the VIDIOC_G_FMT...
    on Apr 30, 2013
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use