This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

OMAP-L138 Booting from SPI ATMEL

Guru 20680 points
Hello, I am using a custom board with OMAP-L138 And SPI flash of ATMEL AT45DB321D. I flashed the SPI using CCS4 with spi-flash-writer( I had to add support for ATMEL since the spi-flash-writer 3.20.00.XX does not include support for atmel). Anyway, I get that the application succeed in reading with the text "File Match". I flashed first arm-spi-ais.bin - "armais" file, but after reseting in mode booting from SPI1 flash (0x0C in boot configuration register), I get no printing at all in UART. I tried to change page size from 528 to 512, and flashed again the armais file but still nothing... Can it be that OMAP cannot boot from ATMEL, or is there anything else wrong in my configuration ? I thank you for your help, Ran Shalit

==========

  • Guru 20680 points

    In reply to Daniel Allred:

    Hi Daniel,

    I have continued the diagnostics today, I see some interesting things:

    1. I am trying to burn only boot-strap meanwhile (without u-boot). As I undestand it should give me some printing in UART anyway, even if u-boot is not flashed. Also if I'm currect I can flash the boot-strap also in other boot modes (not only emulator) since the emulator will always take control on the board. I hope it is OK to work this way.

    2. I see that flashing the SPI flash image/boot-strap/arm-spi-ais.bin does not give me any printings in UART. the disagnotics are at the end of this message. I then tried to flash the bin image of the "flash and boot utils" called ubl_OMAPL138_SPI_MEM.bin. I was surprised to see that the UBL now starts and gives printings in UART , although I get "no magic number is found" in the printings (?). the diagnotics here are the same( except to PC register) for both case.

    3. Same thing as 2 happend when I tried to flash the Nand in my board: flashing the bin from  image/boot-strap/arm-nand-ais.bin gives nothing, but flashing the ubl_OMAPL138_NAND.bin gives printing (UBL works). the diagnotics here are the same( except to PC register) for both cases.

    Any advice is appreciated , Thank you for the help !

    Ran

     

    ARM9_0: Output:  Target Connected.
    ARM9_0: Output:  ---------------------------------------------
    ARM9_0: Output:  Memory Map Cleared.
    ARM9_0: Output:  ---------------------------------------------
    ARM9_0: Output:  Memory Map Setup Complete.
    ARM9_0: Output:  ---------------------------------------------
    ARM9_0: Output:  KICK Unlocked.
    ARM9_0: Output:  ---------------------------------------------
    ARM9_0: Output:  PSC Enable Complete.
    ARM9_0: Output:  ---------------------------------------------
    ARM9_0: Output:  PLL0 init done for Core:300MHz, EMIFA:25MHz
    ARM9_0: Output:  mDDR initialization is in progress....
    ARM9_0: Output:  PLL1 init done for DDR:150MHz
    ARM9_0: Output:  Using mDDR settings
    ARM9_0: Output:  mDDR init for 150 MHz is done
    ARM9_0: Output:  ---------------------------------------------
    ARM9_0: Output:  DSP Wake Complete.
    ARM9_0: Output:  ---------------------------------------------
    ARM9_0: GEL Output:
    ---------------------------------------------
    ARM9_0: GEL Output: |             Device Information            |
    ARM9_0: GEL Output: ---------------------------------------------
    ARM9_0: GEL Output: DEV_INFO_00 = 0x1B7D102F
    ARM9_0: GEL Output: DEV_INFO_01 = 0x00000000
    ARM9_0: GEL Output: DEV_INFO_02 = 0x0000000C
    ARM9_0: GEL Output: DEV_INFO_03 = 0x00000032
    ARM9_0: GEL Output: DEV_INFO_04 = 0x00000000
    ARM9_0: GEL Output: DEV_INFO_05 = 0x000003E0
    ARM9_0: GEL Output: DEV_INFO_06 = 0x00000080
    ARM9_0: GEL Output: DEV_INFO_07-DEV_INFO_08-DEV_INFO_09-DEV_INFO_10-DEV_INFO_11-DEV_INFO_12 = 0-0-5621784-22-46-19
    ARM9_0: GEL Output: DEV_INFO_13,DEV_INFO_14,DEV_INFO_15,DEV_INFO_16 = 2,0,0,11272
    ARM9_0: GEL Output: -----
    ARM9_0: GEL Output: DEV_INFO_17 = 0x00030003
    ARM9_0: GEL Output: DEV_INFO_18 = 0x00000000
    ARM9_0: GEL Output: DEV_INFO_19 =ARM9_0: GEL Output: 0ARM9_0: GEL Output: 0ARM9_0: GEL Output: 0ARM9_0: GEL Output: 0ARM9_0: GEL Output: 0ARM9_0: GEL Output:
    ARM9_0: GEL Output: -----
    ARM9_0: GEL Output: DEV_INFO_20 = 0x30303864
    ARM9_0: GEL Output: DEV_INFO_21 = 0x3630306B
    ARM9_0: GEL Output: DEV_INFO_22 = 0x30303864
    ARM9_0: GEL Output: DEV_INFO_23 = 0x3630306B
    ARM9_0: GEL Output: -----
    ARM9_0: GEL Output: DEV_INFO_24 = 0x1601302E
    ARM9_0: GEL Output: DEV_INFO_25 = 0x0055C818
    ARM9_0: GEL Output: DEV_INFO_06 = 0x00000080
    ARM9_0: GEL Output: DEV_INFO_26 = 0x58100002
    ARM9_0: GEL Output:

    ARM9_0: GEL Output: ---------------------------------------------
    ARM9_0: GEL Output: |               BOOTROM Info                |
    ARM9_0: GEL Output: ---------------------------------------------
    ARM9_0: GEL Output: ROM ID: d800k006
    ARM9_0: GEL Output: Silicon Revision 2.0
    ARM9_0: GEL Output: Boot Mode: SPI1 Flash
    ARM9_0: GEL Output:
    ROM Status Code: 0x00000000
    Description:ARM9_0: GEL Output: No error
    ARM9_0: GEL Output:
    Program Counter (PC) = 0x019482B8
    ARM9_0: GEL Output:
    ARM9_0: GEL Output: ---------------------------------------------
    ARM9_0: GEL Output: |              Clock Information             |
    ARM9_0: GEL Output: ---------------------------------------------
    ARM9_0: GEL Output:
    ARM9_0: GEL Output: PLLs configured to utilize crystal.
    ARM9_0: GEL Output: ASYNC3 = PLL0_SYSCLK2
    ARM9_0: GEL Output:
    ARM9_0: GEL Output: NOTE:  All clock frequencies in following PLL sections are based
    ARM9_0: GEL Output: off OSCIN = 24 MHz.  If that value does not match your hardware
    ARM9_0: GEL Output: you should change the #define in the top of the gel file, save it,
    ARM9_0: GEL Output: and then reload.
    ARM9_0: GEL Output:
    ARM9_0: GEL Output: ---------------------------------------------
    ARM9_0: GEL Output: |              PLL0 Information             |
    ARM9_0: GEL Output: ---------------------------------------------
    ARM9_0: GEL Output:
    ARM9_0: GEL Output: PLL0_SYSCLK1 = 300 MHz
    ARM9_0: GEL Output: PLL0_SYSCLK2 = 150 MHz
    ARM9_0: GEL Output: PLL0_SYSCLK3 = 25 MHz
    ARM9_0: GEL Output: PLL0_SYSCLK4 = 75 MHz
    ARM9_0: GEL Output: PLL0_SYSCLK5 = 300 MHz
    ARM9_0: GEL Output: PLL0_SYSCLK6 = 300 MHz
    ARM9_0: GEL Output: PLL0_SYSCLK7 = 50 MHz
    ARM9_0: GEL Output:
    ARM9_0: GEL Output: ---------------------------------------------
    ARM9_0: GEL Output: |              PLL1 Information             |
    ARM9_0: GEL Output: ---------------------------------------------
    ARM9_0: GEL Output:
    ARM9_0: GEL Output: PLL1_SYSCLK1 = 300 MHz
    ARM9_0: GEL Output: PLL1_SYSCLK2 = 150 MHz
    ARM9_0: GEL Output: PLL1_SYSCLK3 = 300 MHz
    ARM9_0: GEL Output:
    ARM9_0: GEL Output: ---------------------------------------------
    ARM9_0: GEL Output: |              PSC0 Information             |
    ARM9_0: GEL Output: ---------------------------------------------
    ARM9_0: GEL Output:
    ARM9_0: GEL Output: State Decoder:
    ARM9_0: GEL Output:  0 = SwRstDisable (reset asserted, clock off)
    ARM9_0: GEL Output:  1 = SyncReset (reset assered, clock on)
    ARM9_0: GEL Output:  2 = Disable (reset de-asserted, clock off)
    ARM9_0: GEL Output:  3 = Enable (reset de-asserted, clock on)
    ARM9_0: GEL Output: >3 = Transition in progress
    ARM9_0: GEL Output:
    ARM9_0: GEL Output: Module 0: EDMA3CC (0)        STATE = 3
    ARM9_0: GEL Output: Module 1: EDMA3 TC0          STATE = 3
    ARM9_0: GEL Output: Module 2: EDMA3 TC1          STATE = 3
    ARM9_0: GEL Output: Module 3: EMIFA (BR7)        STATE = 3
    ARM9_0: GEL Output: Module 4: SPI 0              STATE = 3
    ARM9_0: GEL Output: Module 5: MMC/SD 0           STATE = 3
    ARM9_0: GEL Output: Module 6: AINTC              STATE = 3
    ARM9_0: GEL Output: Module 7: ARM RAM/ROM        STATE = 3
    ARM9_0: GEL Output: Module 9: UART 0             STATE = 3
    ARM9_0: GEL Output: Module 10: SCR 0 (BR0/1/2/8)  STATE = 3
    ARM9_0: GEL Output: Module 11: SCR 1 (BR4)        STATE = 3
    ARM9_0: GEL Output: Module 12: SCR 2 (BR3/5/6)    STATE = 3
    ARM9_0: GEL Output: Module 13: PRUSS              STATE = 0
    ARM9_0: GEL Output: Module 14: ARM                STATE = 3
    ARM9_0: GEL Output: Module 15: DSP                STATE = 3
    ARM9_0: GEL Output:
    ARM9_0: GEL Output: ---------------------------------------------
    ARM9_0: GEL Output: |              PSC1 Information             |
    ARM9_0: GEL Output: ---------------------------------------------
    ARM9_0: GEL Output:
    ARM9_0: GEL Output: State Decoder:
    ARM9_0: GEL Output:  0 = SwRstDisable (reset asserted, clock off)
    ARM9_0: GEL Output:  1 = SyncReset (reset assered, clock on)
    ARM9_0: GEL Output:  2 = Disable (reset de-asserted, clock off)
    ARM9_0: GEL Output:  3 = Enable (reset de-asserted, clock on)
    ARM9_0: GEL Output: >3 = Transition in progress
    ARM9_0: GEL Output:
    ARM9_0: GEL Output: Module 0: EDMA3CC (1)        STATE = 3
    ARM9_0: GEL Output: Module 1: USB0 (2.0)         STATE = 3
    ARM9_0: GEL Output: Module 2: USB1 (1.1)         STATE = 3
    ARM9_0: GEL Output: Module 3: GPIO               STATE = 3
    ARM9_0: GEL Output: Module 4: UHPI               STATE = 3
    ARM9_0: GEL Output: Module 5: EMAC               STATE = 3
    ARM9_0: GEL Output: Module 6: DDR2 and SCR F3    STATE = 3
    ARM9_0: GEL Output: Module 7: MCASP0 + FIFO      STATE = 3
    ARM9_0: GEL Output: Module 8: SATA               STATE = 3
    ARM9_0: GEL Output: Module 9: VPIF               STATE = 3
    ARM9_0: GEL Output: Module 10: SPI 1              STATE = 3
    ARM9_0: GEL Output: Module 11: I2C 1              STATE = 3
    ARM9_0: GEL Output: Module 12: UART 1             STATE = 3
    ARM9_0: GEL Output: Module 13: UART 2             STATE = 3
    ARM9_0: GEL Output: Module 14: MCBSP0 + FIFO      STATE = 3
    ARM9_0: GEL Output: Module 15: MCBSP1 + FIFO      STATE = 3
    ARM9_0: GEL Output: Module 16: LCDC               STATE = 3
    ARM9_0: GEL Output: Module 17: eHRPWM (all)       STATE = 3
    ARM9_0: GEL Output: Module 18: MMC/SD 1           STATE = 3
    ARM9_0: GEL Output: Module 19: UPP                STATE = 3
    ARM9_0: GEL Output: Module 20: eCAP (all)         STATE = 3
    ARM9_0: GEL Output: Module 21: EDMA3 TC2          STATE = 3
    ARM9_0: GEL Output: Module 24: SCR-F0 Br-F0       STATE = 3
    ARM9_0: GEL Output: Module 25: SCR-F1 Br-F1       STATE = 3
    ARM9_0: GEL Output: Module 26: SCR-F2 Br-F2       STATE = 3
    ARM9_0: GEL Output: Module 27: SCR-F6 Br-F3       STATE = 3
    ARM9_0: GEL Output: Module 28: SCR-F7 Br-F4       STATE = 3
    ARM9_0: GEL Output: Module 29: SCR-F8 Br-F5       STATE = 3
    ARM9_0: GEL Output: Module 30: Br-F7 (DDR Contr)  STATE = 3
    ARM9_0: GEL Output: Module 31: L3 RAM, SCR-F4, Br-F6 STATE = 3

    ==========

  • Guru 20680 points

    In reply to Daniel Allred:

    Hi Daniel,

    In addition to the diagnostic information I gave before, When I compare the difference between the custom board to the EVM, I also see that the device ID in the board is:
    d800k006 - silicon revision 2.0 and in the EVM board: d800k004 - silicon revision 1.1 (difference in bootrom info category), there are also difference in device information category , maybe becuase the device id is different. There is no more difference in the other categories in the diagnostic information.
    As I undestand it is just the revision of the cpu - Meanwhile I have no idea why the custom board behaves different from the EVM.

    Regards,

    Ran

    ==========

  • Guru 20680 points

    In reply to Daniel Allred:

    Hi,

     

    The issue was solved (after debug of UBL)  Any one interested can look at 

    http://e2e.ti.com/support/embedded/f/354/p/113807/405296.aspx#405296

     

    Ran

     

    ==========

  • In reply to ranchu:

    Ran,

    Thanks for providing the update.  I think the lesson here is that the low-level boot loaders can be very much tied to the particulars of the board or platform, and therefore it is very likely that these will need to be customized for a custom platform.

    Regards, Daniel

    ----------------------------------------------------------------------------------------------------------
    Please click the
    Verify Answer button on this post if it answers your question.
    ----------------------------------------------------------------------------------------------------------

     

  • In reply to ranchu:

    Hi Ran:

    We also use AT45DB321D on our custom OMAP-L137 board. How did you add AT45DB321D support to spi-flash-writer? Can you share the modified spi-flash-writer code with us?

    You help is very appreciated!

     

    Jimmy

  • Guru 20680 points

    In reply to jimmy zhang77361:

    Hi jimmy,

    - I don't have now access to the code, maybe tomorrow, but it was very simple: I just took the atmel driver from u-boot (or linux I'm not sure, but probably from u-boot source).
    I also did some very minor changes just to fit into the frame of the spi-flash-writer (not any important change). You should also be aware of the 512/528 bytes issue. When I first tried to flash the Atmel flash it seemed that flashing was done well, but the booting failed. I then figured out that it is becuase the flash came as 528 bytes per page from factory. 

    - I added simple command at start of flash to convert it to 512 bytes per page. That is maybe the only "important" adding to code, I have made. If your flash is 512bytes then you won't need such anyway.

    - Are you working with the updated sdk from TI ? Isn't there still support for the atmel in the spi-flash-writer ? 

    Bye,

    Ran

    ==========

  • In reply to ranchu:

    Hi Ran:

    We have solved the problems and now we can programme AT45DB321D and boot from it. The following is what I have done:

    1. Configure the page size of AT45DB321D-SU to 512 bytes; then did a power cycle;

    2. Modified spi-falsh-writer to support AT45DB321D.

    Thank you very much for your help!

     

    Best regards,

    Jimmy

     

     

  • In reply to jimmy zhang77361:

    Mr. Zhang, could you give modified version of spi-falsh-writer (with support of AT45DB321D)?

    My e-mail: dtp-avb@yandex.ru

    ---

    Thanks at advance.

  • In reply to Alexander Buraga:

    8357.dsp_spi_flash_writer.zipHi Alexander:

     

    1. Configure the page size of AT45DB321D to 512 bytes. The default page size is 528 bytes. You need to configure the page size to 512 bytes. I added the following code in “main.c” of SPI Flash Writer. You need to uncomment the following code in “main.c” the first time.

     

        /*The follow code is to config the page size of AT45DB321D to 512 Byte.*/

    //    Uint8 config_cmd[4] = { 0x3d, 0x2a, 0x80, 0xa6 };

    //    ret = spi_xfer(slave, 32, &config_cmd[0], NULL, SPI_XFER_BEGIN);

    //    if (ret) {

    //          printf("SF: Failed to send config command %02x: %d\n", config_cmd, ret);

    //          return ret;

    //    }   

    //    while(1);    //Added by Jimmy

     

    1. After you build and run the “main.c”, you need to power off the board, then power on the board. Now the page size of AT45DB321D is 512 bytes.
    2. Comment the above code.
    3. Build and run SPI Flash Writer. The you can program the AT45DB321D following the instructions.

     

    The attachment is the modified driver.  

     Please let me know if the code works.

    Best regards,

    Jimmy

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.