This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Connecting a third ADC to OMAP-L138. Where?

Hi,

I'm currently investigating a way to connect a third ADC to the OMAP-L138. I already have 2 ADC (16 bits) connected to the uPP channels, so that can't be used. At first I had in mind a simple SPI ADC connected to a SPI port of the OMAP (and DMA), but after investigation, I found out that it would not really be possible to avoid CPU actions since I don't seem to have a perfect automated control of the SPI chip-select (the ADC I found were using the SCLK for sampling and communication, so the final sampling rate is controlled by the CS).

Then I investigated the McBSP and just found out that maybe VPIF could do it (parallel though). Since this is my first desgin with the OMAP-L138, I though I would ask the community on which option is the best and what is usually used.

My sampling rate is fixed and will be 1M, I prefer serial but can go parallel. I want to use DMA. It's a 12bits ADC.

Thanks!

2 Replies

  • hi DT

    Have you got any solution...I am also working on similar line..can you share your solution...

    hemant

  • In reply to Hemant Chauhan:

    Hi,

    I currently working on another project (urgency). So I don't have a solution at the moment, but when I'll be back on it, I'll gladly share it indeed.

    Sorry,

    DT

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.