Hello
I am rebuiding the sfh_OMAP-L138.exe for my board(DDR2+NOR FLASH 16BIT+25MHZ+UART1),but it only can be used on TI'board(EVM mDDR+SPI FLASH+24MHZ+UART2).
On my board will appear the following error.
E:\>sfh_OMAP-L138.exe -erase -flashType NOR----------------------------------------------------- TI Serial Flasher Host Program for OMAP-L138 (C) 2012, Texas Instruments, Inc. Ver. 1.67-----------------------------------------------------
Platform is Windows. [TYPE] Global erase [TARGET] OMAPL138 [DEVICE] NOR [NOR Block] 0
Attempting to connect to device COM1...Press any key to end this program at any time.
(AIS Parse): Read magic word 0x41504954.(AIS Parse): Waiting for BOOTME... (power on or reset target now)(AIS Parse): BOOTME received!(AIS Parse): Performing Start-Word Sync...(AIS Parse): Performing Ping Opcode Sync...(AIS Parse): Processing command 0: 0x58535901.(AIS Parse): Performing Opcode Sync...(AIS Parse): Loading section...(AIS Parse): Loaded 10792-Byte section to address 0x80000000.(AIS Parse): Processing command 1: 0x58535901.(AIS Parse): Performing Opcode Sync...(Serial Port): Read error! (The operation has timed out.)(AIS Parse): I/O Error in read!(Serial Port): Read error! (The operation has timed out.)(AIS Parse): I/O Error in read!(Serial Port): Read error! (The operation has timed out.)(AIS Parse): I/O Error in read!
what's caused that.??????????????????
waiting for ......................................
Thanks!!!!!
Hi,
The tool present here http://sourceforge.net/projects/dvflashutils/files/OMAP-L138/v2.36/ can also be used for NOR flash.
Thx,
--Prabhakar Lad
HI Prabhakar Lad
The sfh what i used is v2.32 .It supports NOR flash too .I download v2.36 and test it ,but it is erroring too.
Errors like v2.32.
How can i know the operating principle of sfh?
Thanks!
Serial Flasher tool is command-line tool to connect to platform in UART boot mode for writing various flash devices.
You can find the source of it in <tool_directory>/OMAP-L138/GNU/sfh.
Hi
It has been resoved.
Something on board cause the rest of the cpu.
HI, haile zhu. I had similar trouble as you describle here. Now i wanna know what can i do to resolve it?
thanks and looking forward for your reply!