• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » OMAP™ Processors » OMAP-L13x, AM1x and C674x Processors Forum » USB Host controller
Share
OMAP™ Processors
  • Forums
  • Announcements
Options
  • Subscribe via RSS
Resources
  • OMAP-L1x DSP+ARM9™-based Processors Product Folder
  • OMAP3525/30 DSP+ARM Cortex™-A8-based SOCs Product Folder

  • Top OMAPL Wiki Links
  • OMAPL3x Schematic Review Checklist
  • OMAPL13x Boot resources

  • OMAPL Document Resources
  • OMAPL137 Technical reference manual
  • OMAPL138 Technical reference manual
  • OMAPL Boot loader App Notes
  • Forums

    USB Host controller

    This question is not answered
    manuel
    Posted by manuel
    on Sep 03 2008 13:45 PM
    Prodigy110 points

    Hi,

     Did anyone got the USB interface of the OMAP3503 EVM working with Linux ? I want to connect a USB sound card, and it just does nothing.

    I do not get a USB event when I plug in any USB device. Just nothing happens. The USB Host driver is built in, detects one HUB Root,

    but thats it.

     As far as I understand, I need a "Mini A" cable, with the ID pin tied to ground. Can anyone confirm if this is correct ?

     

    Best Regards,

    Manuel

    (Sorry for the wrong post in the DM355 board, I think here maybe is the right place).

     

    USB Linux ALSA
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    All Replies
    • Bernie Thompson TI
      Posted by Bernie Thompson TI
      on Sep 03 2008 15:21 PM
      Mastermind41680 points

      This is indeed the better place for this type of question :) 

      The OMAP35x SDK does provide support for USB devices, and it has been tested, though there are several limitations still present with the USB drivers as discussed in section 2.6 of the PSP release notes.

      You do have to have a MiniA ended cable for this to work, meaning pins 4 and 5 (ID and GND) of the connector are connected together otherwise the port will be in slave mode (i.e. expecting to talk to a master PC as opposed to a slave device).

      You may want to try a powered USB hub, if the USB sound card is drawing more current than the port can handle you may see this type of failure.

      You may also want to try leaving the device connected to the USB when you power cycle the board in case this is some problem with the hotplug event.

      OMAP USB
      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Ajay
      Posted by Ajay
      on Sep 03 2008 23:41 PM
      Genius9470 points

      We have tested OMAP35xx EVM with USB sound card and it works fine."Mini-A" plug is to be inserted on EVM so that EVM can act as USB host. You can try

      $ echo "F" >/proc/driver/musb_hdrc to start a session.

      If my reply answers your question then please click on the green button "Verify Answer"

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Juan Gonzales
      Posted by Juan Gonzales
      on Sep 04 2008 00:23 AM
      Mastermind33965 points

      Please make sure pins 4 and 5 are connected per Bernie's comments above; we did encounter an issue were pins 4 and 5 were not connected together in the USB cable.

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • manuel
      Posted by manuel
      on Sep 04 2008 09:05 AM
      Prodigy110 points

      Hi,

      thanks for the reply. I already had considered all the details posted so far. I also checked the cable if the ID pin was actually connected to ground, and it was as it should be. So the cable is not broken or something like that. Im also using a powered HUB.

      When I do a "cat /proc/driver/musb_hdrc, I get this:

      [root@OMAP3EVM /]# cat /proc/driver/musb_hdrc
      Status: MHDRC, Mode=Host (Power=e0, DevCtl=81)
      OTG state: a_idle; inactive
      Options: musb-dma, host, debug=1 [eps=16]
      Root port status: 00000100

      The OTG status does not look OK for me. Maybe my board is somehow broken ? I'm using the default kernel of the latest SDK (version 1.0.0 I think).

      Any suggestions ?

      Cheers,

      Manuel

      USB Linux
      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • manuel
      Posted by manuel
      on Sep 04 2008 10:34 AM
      Prodigy110 points

       Hi everyone,

       

      It turned out that my OMAP35x board was broken. I tried another different board one, and USB devices are detected just fine. But, it does not work either.

      Either with the original SDK 1.0.0 default kernel or custom kernel with different USB driver settings (experimental code for better transaction handling),

      I get different results for different USB Soundcards:

       

      Gigaport AG: It does not work at all. No audio and error messages and the whole USB stack getting messed up (I have to reboot).

      Maya EX: Stereo works, but 5.1 Output fails, also with error messages and the whole USB stack getting messed up (I have to reboot).

       

      Has anyone got 5.1 Audio working on the OMAP35x EVM and with which audio card ? Thank you in advance.

       

      Cheers,

      Manuel


      USB Linux 5.1
      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Ajay
      Posted by Ajay
      on Sep 05 2008 00:25 AM
      Genius9470 points

      I have tested stereo with TI's DEM-PCM2900/02 card and it works. Let me see if I can get Maya Ex card to test 5.1.

       Regards,

      Ajay

      If my reply answers your question then please click on the green button "Verify Answer"

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • manuel
      Posted by manuel
      on Sep 05 2008 05:22 AM
      Prodigy110 points

       Hi,

       

      but  that TI USB Soundcard seems to support stereo only. Stereo works with the Maya EX also, but 5.1 (6 channels) does not work. It could be a USB bandwidth problem maybe?

      Doing stereo playback on a USB soundcard is quite pointless to me, because I can also do that with the built in audio interface. I'm trying to use the USB soundcard device because I need more audio channels.

       

      Best Regards,

      Manuel

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • swami
      Posted by swami
      on Sep 05 2008 05:47 AM
      Expert7435 points

      Manuel,

      I assume that you are using the aplay utility and the ALSA infrastructure over USB.  I have seen some issues with the kernel USB Audio client driver in this use case.  Have you verified that this driver works say in the PC use case with Maya 5.1 device.  It would be a worthwile option to try out to localise were the issue could be (whether or not it is OMAP specific).  Probably you might have tried it but I could not make it from your posts so far.

       

      swami

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • manuel
      Posted by manuel
      on Sep 05 2008 06:07 AM
      Prodigy110 points

       Hi,

      thanks for replying, but I have been using ALSA for several years (as user, driver and application developer), and I have never had any problems with multichannel. I also have other ARM based systems working just fine with

      the very same audio cards in multichannel mode. I will try using another USB HUB, see what happens, maybe its a signal integrity problem?


      Cheers,

      Manuel


      USB Linux ALSA
      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • swami
      Posted by swami
      on Sep 05 2008 08:06 AM
      Expert7435 points

      Good to know that you are familiar with the ALSA infrastructure quite a bit.   

      We had an issue with the usbaudio.c code in "sound/usb" directory were the USB flags were not correctly updated.  This lead to random oops after recording stopped.  We corrected the issue by correctly updating the ASYNC flag in the URB flags structure.  Need to post the patch to the community though.  Busy with other tasks now will do so shortly.  This is based on the 2.6.27 OMAP GIT code ( we back ported it to 2.6.10 kernel but the fix I think applies equally on both kernel versions).  That is the reason I mentioned there could be probable issues in the ALSA Sound driver.

      Have you encountered the above issue by any chance ?

       

      swami

      USB Linux ALSA
      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • manuel
      Posted by manuel
      on Sep 05 2008 11:46 AM
      Prodigy110 points

       Hi,

       Thanks for the information. I did some googling about that. Does this problem show up under any circumstance or only if I request explicitly the ASYNC mehtod ? The error message that is supposed to reveal this problem seems to be "file descriptor in wrong state" or something like that. I have NOT encountered that error message. I would be glad if I could try a workaround to that issue. Do you have any diff patch around which you could take a look at ?

       Cheers,

      Manuel

      USB Linux ALSA
      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • swami
      Posted by swami
      on Sep 05 2008 12:27 PM
      Expert7435 points

      Manuel,

      By default the async flag is set to 1 in the kernel build.  Would try to post the patch by next week.

       swami

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • manuel
      Posted by manuel
      on Sep 13 2008 12:32 PM
      Prodigy110 points

      Hi Swami,

      Would it it be of any help as a work around to use some API call to force ASYNC=0 or something like that ? How ever if you could post a patch would be really great.

      Best Regards,

      Manuel

       

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • manuel
      Posted by manuel
      on Sep 25 2008 08:01 AM
      Prodigy110 points

      Hi there,

      Here are the error messages I get as soon as I try to play back a 6 channel 48KHz 16 bit resolution WAV file using aplay:

      usbhid 1-1.4:1.3: usb_probe_interface
      usbhid 1-1.4:1.3: usb_probe_interface - got id
      input: USB Audio as /class/input/input2
      input: USB HID v1.00 Device [USB Audio] on usb-musb_hdrc.0-1.4
      drivers/usb/core/inode.c: creating file '008'
      usb_endpoint usbdev1.8_ep01: ep_device_release called for usbdev1.8_ep01
      musb_stage0_irq 722: BUS RESET
      usb 1-1.4: aplay timed out on ep0out len=0/0
      musb_h_tx_flush_fifo 126: Could not flush host TX fifo: csr: 000a
      usb 1-1.4: aplay timed out on ep0out len=0/0
      musb_h_tx_flush_fifo 126: Could not flush host TX fifo: csr: 000a
      8:1:2: usb_set_interface failed

      The USB sound card does not support resampling, so I cannot test lower sample rates in order to sort out bandwidth problems.

      Any ideas ?

      Best Regards,

      Manuel Jander

       

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Juan Gonzales
      Posted by Juan Gonzales
      on Sep 25 2008 10:43 AM
      Mastermind33965 points

      My initial thought is that our SDK drivers (which I assume you are using) are written for the Mistral OMAP35x EVM, which only supports stereo 2-channel output.  I do not believe the hardware (and probably Linux drivers) can handle 6-channels.

      OMAP35xx AUDIO
      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    12
    TI E2E™ Community
    • Support Forums
    • Blogs
    • Videos
    • Groups
    • Site Support & Feedback
    • Settings
    TI E2E™ Community Groups
    • TI University Program
    • Make the Switch
    • Microcontroller Projects
    • Motor Drive & Control
    Other Communities
    • Deyisupport
    • Designsomething.org
    • beagleboard.org
    • TI on Element 14
    • TI on TechXchangeSM
    Other Technical & Support Resources
    • WEBENCH® Design Center
    • Product Information Centers
    • Technical Documents
    • TI Design Network
    • TI Technical Articles
    • TI Training

    All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

    Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

    Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
    TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

    TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
    embedded processors, along with software, tools and the industry’s largest sales/support staff.

    © Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
    Trademarks | Privacy Policy | Terms of Use