This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OMAP-L138
Hi,
I'm working on a custom-manufactured board with OMAP-L138 processor and a Spartan-6 FPGA. The ARM and DSP cores run Linux and SYS/BIOS, respectively.
I'm able to SysLink Notify API to send interrupts between the cores. On the other hand, I also need the DSP to get interrupts from the FPGA through uPP; to that end, I have a code that uses the "interrupt.h" API to register ISRs for uPP events.
However, when I call IntRegister(), IntEventMap(), and IntEnable() functions, the Notify API stops responding. I changed the CPUint parameter to see if that'll solve the problem, but it didn't.
Are these two APIs incompatible? How can I register for both ARM-side (Notify) events and FPGA-side (uPP) events from the DSP?
Is there a way to send and receive to/from the ARM (running Linux) without using the Notify module?
Thanks in advance.
(Btw, I know SysLink has been replaced by IPC 3.x, but SysLink is the recommended IPC method in the TI Wiki and it is included by default in OMAP-L138 Multi-Core SDK.)
Edit: After investigating, I realized it is IntDSPINTCinit() that causes SysLink Notify to crash. However, if I comment it out, then SysLink will work, but uPP will stop working. Any ideas?
In reply to Lalindra Jayatilleke:
I realized the line "ISTP = (unsigned int)_intcVectorTable;" appears to be what breaks the SysLink Notify module. After setting ISTP, I can't initialize the Notify module properly and IPC interrupts won't work.
Could you please help me solve this problem?
Silacko
In reply to silacko:
--------------------------------------------------------------------------------------------------------------------------------------Please click the This resolved my issue button on this post if the responses on this E2E thread answers your question.--------------------------------------------------------------------------------------------------------------------------------------